Question
STM32H573xx: update with ST-JLINK
In the case of a root of trust with two boot stages (STiRoT + OEMuRoT), I'm looking to update the OEMuRoT or the firmware. From STM32CubeProgrammer I can do this via the bootloader. However, when I use the ST-LINK probe and try to program the new firmware (the encrypted and signed hex that worked in the case of the bootloader) I get the following error: ‘failed to download firmware’.
I am in PRODUCT_STATE = OPEN

the logs indicate that the flash cannot be programmed
Is it possible to update encrypted and signed firmware using the ST-LINK probe?