Skip to main content
Associate II
Nov 5, 2024 8:50 AM UTC
Solved

STM32H573 stuck in PROVISIONING state

Hi there,

My STM32H573I-DK demo board is stuck in PROVISIONING state, probably as the result of a failed or aborted provisioning operation. I was doing hand-on training  with the  How to start with STiRoT on STM32H573 wiki.

 

Now, I cannot regress it to OPEN, or run the provisioning.sh script again to proceed to CLOSED. Any attempt ends up in a Debug Authentication Failed error.

I am aware of the importance of providing DA credentials to avoid locking the device in CLOSED state. But I don't think I missed this step, and my device is not CLOSED.

 

Any idea how I can unlock this board ?

Thanks for any support.

Christian R

 

FYI, here is the log of a regression attempt using STM32Programmer:

09:34:22 : STM32CubeProgrammer API v2.17.0 | Linux-64Bits
09:34:40 : Start Debug Authentication Sequence
09:34:40 : SDMOpen : 609 : open : SDM API v1.0
09:34:40 : SDMOpen : 610 : open : SDM Library version v1.1.0
09:34:40 : open_comms : 501 : open : Asserting target reset
09:34:40 : open_comms : 505 : open : Writing magic number
09:34:40 : open_comms : 515 : open : De-asserting target reset
09:34:40 : open_comms : 567 : open : Communication with the target established successfully
09:34:40 : discovery: target ID.......................:0x484
09:34:40 : discovery: SoC ID..........................:0x00000000_35353537_3332510A_00680036
09:34:40 : discovery: SDA version.....................:2.4.0
09:34:40 : discovery: Vendor ID.......................:STMicroelectronics
09:34:40 : discovery: PSA lifecycle...................:ST_LIFECYCLE_PROVISIONING
09:34:40 : discovery: PSA auth version................:1.0
09:34:40 : discovery: ST HDPL1 status.................:0xffffffff
09:34:40 : discovery: ST HDPL2 status.................:0xffffffff
09:34:40 : discovery: ST HDPL3 status.................:0xffffffff
09:34:40 : discovery: Token Formats...................:0x200
09:34:40 : discovery: Certificate Formats.............:0x201
09:34:40 : discovery: cryptosystems...................:Ecdsa-P256 SHA256
09:34:40 : discovery: ST provisioning integrity status:0xf5f5f5f5
09:34:40 : discovery: permission if authorized...........:Full Regression
09:34:40 : discovery: permission if authorized...........:To TZ Regression
09:34:40 : discovery: permission if authorized...........:Level 3 Intrusive Debug
09:34:40 : discovery: permission if authorized...........:Level 2 Intrusive Debug
09:34:40 : discovery: permission if authorized...........:Level 1 Intrusive Debug
09:34:40 : discovery: permission if authorized...........:Level 3 Intrusive Non Secure Debug
09:34:40 : discovery: permission if authorized...........:Level 2 Intrusive Non Secure Debug
09:34:40 : discovery: permission if authorized...........:Level 1 Intrusive Non Secure Debug
09:35:11 : Start Debug Authentication Sequence
09:35:11 : SDMOpen : 609 : open : SDM API v1.0
09:35:11 : SDMOpen : 610 : open : SDM Library version v1.1.0
09:35:11 : open_comms : 501 : open : Asserting target reset
09:35:11 : open_comms : 505 : open : Writing magic number
09:35:11 : open_comms : 515 : open : De-asserting target reset
09:35:11 : open_comms : 567 : open : Communication with the target established successfully
09:35:11 : [00%] discovery command
09:35:11 : [10%] sending discovery command
09:35:11 : [20%] receiving discovery
09:35:11 : [40%] loading credentials
09:35:11 : [50%] sending challenge request
09:35:11 : [60%] receiving challenge
09:35:11 : Error: Debug Authentication Failed

This topic has been closed for replies.
Frantz LEFRERE
Frantz LEFREREBest answer
ST Technical Moderator
Nov 5, 2024 12:35 PM UTC

Hi @CRE ,

please do the provisioning with the DA_Config.obk from the archive attached and then do the regression with the cert_root.b64 from the archive with cubeprogrammer.
I would suspect that you've regenerated the root key but haven't regenerated the associated certificate.

Br,

Frantz 

4 replies

Frantz LEFRERE
ST Technical Moderator
Nov 5, 2024 9:17 AM UTC

Hello @CRE 
As you are in provisioning state, you can still doing the provisioning manually.
Launch cube programmer GUI, connect in hotplug mode.
Then click on the shield, select the DA_config.obk ( from the Cube) and start provisioning.
Manual_provisioning.JPG
Then you should have a pop-up that the povsioning was success full.
Once this done the regression script could be launch.
Or you can do the regression thank cube programmer GUI.

Br,

Frantz

CREAuthor
Associate II
Nov 5, 2024 10:58 AM UTC

Hi Frantz,

Thank you a lot for the quick and detailed answer.

I put your suggestion to trial:

- manual provisioning : appeared to be successful. Yet, the device was still in PROVISIONING state after that.

- regression : with the script or from STM32Programmer, both failed. The process went a bit further than before (signing token):

CRE_0-1730803547346.png

 

Frantz LEFRERE
Frantz LEFREREBest answer
ST Technical Moderator
Nov 5, 2024 12:35 PM UTC

Hi @CRE ,

please do the provisioning with the DA_Config.obk from the archive attached and then do the regression with the cert_root.b64 from the archive with cubeprogrammer.
I would suspect that you've regenerated the root key but haven't regenerated the associated certificate.

Br,

Frantz