STM32H573 STiROT+OEMuROT example failed provisioning.
- 15 replies
- 336 views
Hi Community,
I’m provisioning an STM32H573 (installed on a NUCLEO-H563ZI board; I replaced H563 with H573). I followed the ST example STiRoT_OEMuROT from STM32Cube FW H5 v1.6.0. During provisioning the script aborts with:
Error when trying to Set SECBOOT_LOCK option byte to 0xC3 (unlock secure boot address)
Provisioning aborted.
Environment:
- MCU: STM32H573 (2 MB flash)
- Host tools: STM32_Programmer_CLI v2.19.0
- Product state chosen in provisioning script: OPEN.
after i read the option bytes using STM32_Programmer_CLI -c port=SWD -ob displ
i found that,
Product state:
PRODUCT_STATE: 0xED (Open)
BOR Level:
BOR_LEV : 0x0 (BOR Level 1, the threshold level is low (around 2.1 V))
BORH_EN : 0x0 (0x0)
User Configuration:
IO_VDD_HSLV : 0x0 (0x0)
IO_VDDIO2_HSLV: 0x0 (0x0)
IWDG_STOP : 0x1 (0x1)
IWDG_STDBY : 0x1 (0x1)
BOOT_UBE : 0xC3 (ST-iRoT (system flash) selected)
SWAP_BANK : 0x0 (0x0)
IWDG_SW : 0x1 (0x1)
NRST_STOP : 0x1 (0x1)
NRST_STDBY : 0x1 (0x1)
OPTION BYTES BANK: 1
User Configuration 2:
TZEN : 0xB4 (Trust zone enabled)
USBPD_DIS : 0x1 (Disabled)
SRAM2_ECC : 0x0 (SRAM2 ECC check enabled )
SRAM3_ECC : 0x1 (SRAM3 ECC check disabled)
BKPRAM_ECC : 0x1 (BKPRAM ECC check disabled)
SRAM2_RST : 0x0 (SRAM2 erase when system reset)
SRAM1_3_RST : 0x1 (SRAM1 and SRAM3 not erased when a system reset occurs)
OPTION BYTES BANK: 2
Boot Configuration:
NSBOOTADD : 0x80000 (0x8000000)
NSBOOT_LOCK : 0xC3 (The SWAP_BANK and NSBOOTADD can still be modified following their individual rules.)
SECBOOT_LOCK : 0xB4 (The BOOT_UBE and SECBOOTADD are frozen. SWAP_BANK can only be modified with TZEN set to 0xC3 (disabled).)
SECBOOTADD : 0xC0004 (0xC000400)
OPTION BYTES BANK: 3
also, when device goes in boot mode, i am not able to read the option bytes, for reading the option bytes i have to remove boot0 pin from VDD and reset it.
STM32_Programmer_CLI -c port=SWD mode=HOTPLUG -ob displ
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
ST-LINK SN : 004700463434511634313937
ST-LINK FW : V3J17M10
Board : NUCLEO-H563ZI
Voltage : 3.28V
Error: Unable to get core ID
Error: Cannot connect to access port 1!
If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode.
If you are trying to connect to a device which supports Debug Authentication with certificate or password, please open your device using it.
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 004700463434511634313937
ST-LINK FW : V3J17M10
Board : NUCLEO-H563ZI
Voltage : 3.29V
Error: Unable to get core ID
Error: Cannot connect to access port 1!
If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode.
If you are trying to connect to a device which supports Debug Authentication with certificate or password, please open your device using it.
Question: what’s preventing `SECBOOT_LOCK=0xC3` from being written? Is it:
- OB protected because ST-iRoT is running and re-writing OBs?
- some required precondition in option bytes I haven’t met?
- needing a different connect sequence (Hotplug/hardRst) or specific CLI version?
also, Please find an attached logs of obkey_provision.log