Skip to main content
Associate
July 28, 2026
Question

STM32H563 Provisioning (0x17) - Debug Authentication Discovery Works, Full Regression Fails

Hello ST Community,

I have an STM32H563 (Rev X) that appears to be stuck in the Provisioning state and I am trying to recover it.

Hardware / Tools

MCU : STM32H563

Device ID : 0x484

Revision : Rev X

STM32CubeProgrammer : v2.23.0

Probe : ST-LINK V3SET

ST-LINK FW : V3J16M9B5S1

 

NRST is connected to the ST-LINK and Debug Authentication discovery is working.

Current Option Bytes

PRODUCT_STATE = 0x1

TZEN = 0xB4 (TrustZone enabled)

BOOT_UBE = 0xB4 (OEM-iRoT selected)

SECWM1_STRT = 0x0

SECWM1_END = 0x7F

SECWM2_STRT = 0x0

SECWM2_END = 0x7F

WRPSGn1 = 0xFFFFFFFF

WRPSGn2 = 0xFFFFFFFF

LOCKBL = 0x0

HDP1_STRT = 0x1

HDP1_END = 0x0

HDP2_STRT = 0x1

HDP2_END = 0x0

 

Symptoms

I can: 

- connect through ST-LINK V3

- read option bytes

- read flash

- erase sectors

I cannot:

- perform Mass Erase

- change PRODUCT_STATE back to 0xED

 

Attempting: PRODUCT_STATE = 0xED results in:

Expected value for Option Byte "PRODUCT_STATE": 0xED

found: 0x17

Option Byte Programming failed

Or modified by application after OB_LAUNCH

 

Debug Authentication Discovery

Using:

STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG reset=HWrst debugauth=2

I get:

PSA lifecycle...................: ST_LIFECYCLE_PROVISIONING

 

cryptosystems...................: Ecdsa-P256 SHA256

 

ST provisioning integrity status: 0xEAEAEAEA

ST provisioning integrity status message: VALID

 

permission if authorized........: Full Regression

permission if authorized........: To TZ Regression

Discovery completes successfully.

Debug Authentication Discovery succeeds only after connecting NRST to ST-LINK V3SET.

 

Debug Authentication

Using: 

STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG reset=HWrst debugauth=1

I provide:

key_3_leaf.pem

cert_leaf_chain.b64

from:

STM32CubeProgrammer\bin\DA_Default_Config\STM32H5

Authentication progresses to:

Found 3 certificates

Signing token

but ends with:

Timeout while receiving response...

Debug Authentication Failed

This happens for both:

(a) Full Regression

(b) To TZ Regression

 

Additional Information

Earlier I used:

Reset MCU to Factory Settings

and CubeProgrammer reported:

Provisioning using default ST defined DA-Config PASSED

Performing discovery and regression PASSED

After that the device remained in:

PRODUCT_STATE = 0x17

and Debug Authentication became discoverable.

 

Questions

  1. Is there a known recovery procedure for an STM32H563 in 

    PRODUCT_STATE = 0x17 ST_LIFECYCLE_PROVISIONING  when DA Discovery succeeds but DA Authentication fails?

  2. Are the default files: 

    key_3_leaf.pem and cert_leaf_chain.b64 expected to work with the DA configuration installed by "Reset MCU to Factory Settings"?

  3. Is there a way to determine which certificate chain/root key is currently provisioned in the device?

  4. Is the device recoverable through Full Regression or is another provisioning step required first? 

Any help would be greatly appreciated.

Thanks!

2 replies

Jocelyn RICARD
ST Employee
July 29, 2026

Hello ​@FransMo ,

you probably forgot to connect the NRST pin to the STlink.This is required for DA.

Best regards 

Jocelyn

FransMoAuthor
Associate
July 30, 2026

Hi Jocelyn,

I have the NRST pin already connected to the STlink, no results.

Kind regards,

Frans