Skip to main content
Associate II
September 9, 2025
Solved

stm32h533 production state closed firmware not running

  • September 9, 2025
  • 2 replies
  • 1082 views

Hello Support Team,

for testing purposes i am using the H533NucleoBoard. I can load my firmware into the MCU and the firmware is running as expected. I want use the final product in ProductionState: closed.

The problem is, the firmware isn't running any longer whe changing the productionState to closed. But I am able to switch back to ProductionState: open  via Regression.

Following informations:

Used Tools: Stm32CubeProgrammer V2.20.0

STLink V3 FirmwareVersion: V3J16M8

Following Settings:

TZEN: C3 (disabled) (I don't want to use TrusZone enabled)

BOOT_UBE: B4 (OEM-iRot UserFlash)

NSBOOT_LOCK : C3

SECBOOT_LOCK : 0

Sequence:

1. set product state: Provisioning

2. start provisioning

3. set product state: closed

LogFile of Provisioning process:

06:55:11:421 : reset ap 1
06:55:11:421 : Reset MCU
06:55:11:422 : Reconnecting...
06:55:11:422 : Disconnected
06:55:11:422 : ST-LINK SN : 0019002A3433511537363934
06:55:11:423 : ST-LINK FW : V3J16M8
06:55:11:423 : Board : NUCLEO-H533RE
06:55:11:423 : Voltage : 3.30V
06:55:11:423 : SWD freq : 8000 KHz
06:55:11:423 : Connect mode: Hot Plug
06:55:11:423 : Reset mode : Hardware reset
06:55:11:423 : Device ID : 0x478
06:55:11:423 : Revision ID : --
06:55:11:423 : Reconnected !
06:55:11:424 : Secure Data Provisioning Start. OBK Input file : C:\STM32H533-H573_ConfigWithPassword.obk
06:55:11:424 : ObKey::Reading STM32 descriptor ...
06:55:11:424 : STM32 Descriptor successfully read
06:55:11:424 : Programming via Debugger!
06:55:11:426 : Programming via Debugger!
06:55:11:426 : Core is not halted. Core will be halted.
06:55:11:426 : halt ap 1
06:55:11:426 : r ap 1 reg 0 0x200033E0
06:55:11:426 : r ap 1 reg 1 0x10000000
06:55:11:427 : r ap 1 reg 2 0x00000000
06:55:11:427 : r ap 1 reg 3 0x00000000
06:55:11:427 : r ap 1 reg 4 0x40005C00
06:55:11:427 : r ap 1 reg 5 0x00000000
06:55:11:427 : r ap 1 reg 6 0x00000000
06:55:11:427 : r ap 1 reg 7 0x00000000
06:55:11:427 : r ap 1 reg 8 0x00000000
06:55:11:427 : r ap 1 reg 9 0x00000000
06:55:11:427 : r ap 1 reg 10 0x00000000
06:55:11:427 : r ap 1 reg 11 0x00000000
06:55:11:427 : r ap 1 reg 12 0x00000005
06:55:11:428 : r ap 1 SP 13 0x20003BC8
06:55:11:428 : r ap 1 LR 14 0x0BF9EF63
06:55:11:428 : r ap 1 PC 15 0x0BF9E91C
06:55:11:428 : r ap 1 XPSR 16 0x01004800
06:55:11:428 : r ap 1 MSP - 0x20003BC8
06:55:11:428 : r ap 1 PSP - 0x20003BE0
06:55:11:428 : r ap 1 CR 20 0x00000000
06:55:11:429 : halt ap 1
06:55:11:429 : run ap 1
06:55:11:429 : halt ap 1
06:55:11:429 : OBKey Provisioned successfully C:\STM32H533-H573_ConfigWithPassword.obk
06:55:48:902 : Option byte command : -ob PRODUCT_STATE=114
06:55:48:903 : UPLOADING ...
06:55:48:903 : Size : 4 Bytes
06:55:48:903 : Address : 0x40022050
06:55:48:905 : Read progress:
06:55:48:905 : Data read successfully
06:55:48:905 : Time elapsed during the read operation is: 00:00:00.001
06:55:48:907 : qCmd : -ob PRODUCT_STATE=114
06:55:48:908 : PROGRAMMING OPTION BYTES AREA ...
06:55:48:911 : halt ap 1
06:55:48:911 : r ap 1 reg 15 PC 0x20034000
06:55:48:911 : run ap 1
06:55:48:929 : Database: Config 0 is active.
06:55:48:930 : Bank : 0x00
06:55:48:930 : Address : 0x40022050
06:55:48:930 : Size : 8 Bytes
06:55:48:931 : halt ap 1
06:55:48:948 : reset ap 1
06:55:48:948 : Reset MCU
06:55:48:949 : Reconnecting...
06:55:50:077 : ST-LINK SN : 0019002A3433511537363934
06:55:50:077 : ST-LINK FW : V3J16M8
06:55:50:078 : Board : NUCLEO-H533RE
06:55:50:078 : Voltage : 3.30V
06:55:50:187 : Error: Unable to get core ID
06:55:50:187 : Error: Cannot connect to access port 1! If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode. If you are trying to connect to a device which supports Debug Authentication with certificate or password, please open your device using it.
06:55:50:187 : ...retrying...
06:55:50:722 : ST-LINK SN : 0019002A3433511537363934
06:55:50:722 : ST-LINK FW : V3J16M8
06:55:50:722 : Board : NUCLEO-H533RE
06:55:50:723 : Voltage : 3.30V
06:55:50:832 : Error: Unable to get core ID
06:55:50:833 : Error: Cannot connect to access port 1! If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode. If you are trying to connect to a device which supports Debug Authentication with certificate or password, please open your device using it.
06:55:50:833 : ...retrying...
06:55:51:359 : ST-LINK SN : 0019002A3433511537363934
06:55:51:359 : ST-LINK FW : V3J16M8
06:55:51:360 : Board : NUCLEO-H533RE
06:55:51:361 : Voltage : 3.30V
06:55:51:470 : Error: Unable to get core ID
06:55:51:471 : Error: Cannot connect to access port 1! If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode. If you are trying to connect to a device which supports Debug Authentication with certificate or password, please open your device using it.
06:55:51:471 : ...retrying...
06:55:51:991 : ST-LINK SN : 0019002A3433511537363934
06:55:51:991 : ST-LINK FW : V3J16M8
06:55:51:992 : Board : NUCLEO-H533RE
06:55:51:993 : Voltage : 3.30V
06:55:52:102 : Error: Unable to get core ID
06:55:52:103 : Error: ST-LINK error (DEV_TCP_CMD_ERR)
06:55:52:104 : ...retrying...
06:55:52:627 : ST-LINK SN : 0019002A3433511537363934
06:55:52:627 : ST-LINK FW : V3J16M8
06:55:52:628 : Board : NUCLEO-H533RE
06:55:52:628 : Voltage : 3.30V
06:55:52:736 : Error: Unable to get core ID
06:55:52:737 : Error: ST-LINK error (DEV_TCP_CMD_ERR)
06:55:52:737 : ...retrying...
06:55:53:265 : ST-LINK SN : 0019002A3433511537363934
06:55:53:265 : ST-LINK FW : V3J16M8
06:55:53:267 : Board : NUCLEO-H533RE
06:55:53:267 : Voltage : 3.30V
06:55:53:375 : Error: Unable to get core ID
06:55:53:376 : Error: ST-LINK error (DEV_TCP_CMD_ERR)
06:55:53:376 : Error: failed to reconnect after reset !
06:55:55:529 : Database: Config 6 is active.
06:55:55:529 : Error: Unable to reconnect after setting the Option Bytes
06:55:56:312 : Error: Unable to get core ID
06:55:56:313 : fail @0xFEEEFEEE
06:55:56:314 : Error: Unable to get core ID
06:55:56:314 : Error: Unable to get core ID
06:55:56:314 : Warning: Connection to device 0x478 is lost
06:55:56:328 : Disconnected
06:55:56:328 : Disconnected from device.

 

//LogFile of Regression

07:02:30 : STM32CubeProgrammer API v2.20.0 | Windows-64Bits
07:02:44 : Start Debug Authentication Sequence
07:02:44 : SDMOpen : 624 : open : SDM API v1.0
07:02:44 : SDMOpen : 625 : open : SDM Library version v1.2.0
07:02:44 : open_comms : 513 : open : Asserting target reset
07:02:44 : open_comms : 517 : open : Writing magic number
07:02:44 : open_comms : 537 : open : De-asserting target reset
07:02:44 : open_comms : 584 : open : Communication with the target established successfully
07:02:44 : discovery: target ID.......................:0x478
07:02:44 : discovery: SoC ID..........................:0x00000000_32313831_33335101_00530049
07:02:44 : discovery: SDA version.....................:1.2.0
07:02:44 : discovery: Vendor ID.......................:STMicroelectronics
07:02:44 : discovery: PSA lifecycle...................:ST_LIFECYCLE_CLOSED
07:02:44 : discovery: PSA auth version................:1.0
07:02:44 : discovery: ST HDPL1 status.................:0xffffffff
07:02:44 : discovery: ST HDPL2 status.................:0xffffffff
07:02:44 : discovery: ST HDPL3 status.................:0xffffffff
07:02:44 : discovery: Token Formats...................:0x200
07:02:44 : discovery: Certificate Formats.............:0x201
07:02:44 : discovery: cryptosystems...................:ST Password
07:02:44 : discovery: ST provisioning integrity status:0xeaeaeaea
07:02:44 : discovery: permission if authorized...........:Full Regression
07:02:58 : UR connection mode is defined with the HWrst reset mode
07:02:58 : UR connection mode is defined with the HWrst reset mode
07:02:58 : Start Debug Authentication Sequence
07:02:58 : SDMOpen : 624 : open : SDM API v1.0
07:02:58 : SDMOpen : 625 : open : SDM Library version v1.2.0
07:02:58 : open_comms : 513 : open : Asserting target reset
07:02:58 : open_comms : 517 : open : Writing magic number
07:02:58 : open_comms : 537 : open : De-asserting target reset
07:02:58 : open_comms : 584 : open : Communication with the target established successfully
07:02:58 : [00%] discovery command
07:02:58 : [10%] sending discovery command
07:02:58 : [20%] receiving discovery
07:02:58 : [40%] loading credentials
07:02:58 : [50%] sending challenge request
07:02:58 : [60%] receiving challenge
07:02:58 : SDMAuthenticate : 1391 : client : Found 1 certificates
07:02:58 : [80%] sending ST password
07:02:58 : [90%] receiving response
07:02:58 : [100%] authentication successful
07:02:58 : SDMAuthenticate : 1456 : client : Authentication successful
07:02:58 : Debug opened successfully. the target will be connected.
07:02:58 : Disconnected from device.
07:02:58 : ST-LINK SN : 0019002A3433511537363934
07:02:58 : ST-LINK FW : V3J16M8
07:02:58 : Board : NUCLEO-H533RE
07:02:58 : Voltage : 3.31V
07:02:58 : SWD freq : 8000 KHz
07:02:58 : Connect mode: Under Reset
07:02:58 : Reset mode : Hardware reset
07:02:58 : Device ID : 0x478
07:02:58 : Revision ID : --
07:02:58 : Debug in Low Power mode enabled.
07:02:58 : SFSP Version: v1.2.0
07:02:59 : UPLOADING OPTION BYTES DATA ...
07:02:59 : Bank : 0x00
07:02:59 : Address : 0x40022050
07:02:59 : Size : 8 Bytes
07:02:59 : Bank : 0x01
07:02:59 : Address : 0x40022070
07:02:59 : Size : 16 Bytes
07:02:59 : Bank : 0x02
07:02:59 : Address : 0x40022080
07:02:59 : Size : 16 Bytes
07:02:59 : Bank : 0x03
07:02:59 : Address : 0x400220e0
07:02:59 : Size : 16 Bytes
07:02:59 : Bank : 0x04
07:02:59 : Address : 0x400221e0
07:02:59 : Size : 16 Bytes
07:02:59 : Bank : 0x05
07:02:59 : Address : 0x40022090
07:02:59 : Size : 8 Bytes
07:02:59 : Bank : 0x06
07:02:59 : Address : 0x400220f0
07:02:59 : Size : 8 Bytes
07:02:59 : Bank : 0x07
07:02:59 : Address : 0x400221f0
07:02:59 : Size : 8 Bytes
07:02:59 : Bank : 0x08
07:02:59 : Address : 0x400220f8
07:02:59 : Size : 8 Bytes
07:02:59 : Bank : 0x09
07:02:59 : Address : 0x400221f8
07:02:59 : Size : 8 Bytes
07:02:59 : UPLOADING ...
07:02:59 : Size : 1024 Bytes
07:02:59 : Address : 0x8000000
07:02:59 : Read progress:
07:02:59 : Data read successfully
07:02:59 : Time elapsed during the read operation is: 00:00:00.012

 

I have no idea, what I am doing wrong.

Maybe anyone can help me.

Thanks in advance.

best regards

jhoerd

 

 

 

 

 

 

 

 

 

 

This topic has been closed for replies.
Best answer by Jocelyn RICARD

Hello @jhoerd ,

If your application starts correctly after power on in OPEN state, the only reason I know it could fail when you close the device is because you use the  the DWT->CYCCNT for some timeout.

The DWT as well as all debug peripherals are not available when product is closed.

Best regards

Jocelyn

 

2 replies

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
September 9, 2025

Hello @jhoerd ,

If your application starts correctly after power on in OPEN state, the only reason I know it could fail when you close the device is because you use the  the DWT->CYCCNT for some timeout.

The DWT as well as all debug peripherals are not available when product is closed.

Best regards

Jocelyn

 

jhoerdAuthor
Associate II
September 10, 2025

Hello Jecelyn,

thank you very  much for your advice. Not using DWT->CYCCNT has solved my problem.

thanks again.

Best regards

jhoerd