Skip to main content
Explorer II
July 22, 2026
Question

STM32H5: OEMiROT App installation using swap method

Hi,

I am using the Nucleo H563ZI for OEMiROT. I was able to build the example provided in STM32CubeH5 package and it works without issue. I wanted to know if it is possible to use the swap method instead of overwrite method for the application installation. If so, is there any example available? I understand that HW crypto isnt available on the STM32H563ZI, I was planning to use the ST Cryptolib library for software crypto.

Thanks!

Rajas

1 reply

mƎALLEm
ST Technical Moderator
July 22, 2026

Hello ​@rajasjoshi ,

Crypto and security related questions need to be posted in STM32 MCUs Security forum board.

I moved it now.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.