Skip to main content
NKorn.12
Associate
Sep 30, 2019 12:04 PM UTC
Question

STM32F412 CRC32 uint8_t array as input.

Hi,

I have (for example) a byte array with the size of 6. Now I want to calculate its crc32 value. The first 4 bytes are no problem - I put them in as word, but what about the last 2 bytes?

Thanks for the Help in advance.

BR

Nico

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Sep 30, 2019 12:08 PM UTC

The HW CRC on the part operates on 32-bit at a time. To handle odd bytes you must either use consistent padding bytes or work the smaller amounts​ in SW.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Sep 30, 2019 2:50 PM UTC
uint32_t CrcCCITTBytes(const uint8_t * data, uint32_t size);
 uint32_t CrcCCITTBytes(const uint8_t * data, uint32_t size) {
 uint32_t i;
 CRC->CR = CRC_CR_RESET;
 while(CRC->CR & CRC_CR_RESET); // avoiding the not-reset-fast-enough bug
 i = size % 4;
 switch(i) {
 case 0:
 break;
 case 1:
 CRC->DR = 0xFFFFFFB9;
 CRC->DR = 0xAF644900
 | (__RBIT(*(uint32_t*)(uintptr_t)&data[0]) >> 24)
 ;
 break;
 case 2:
 CRC->DR = 0xFFFFB950;
 CRC->DR = 0x64490000
 | (__RBIT(*(uint32_t*)(uintptr_t)&data[0]) >> 16)
 ;
 break;
 case 3:
 CRC->DR = 0xFFB9509B;
 CRC->DR = 0x49000000
 | (__RBIT(*(uint32_t*)(uintptr_t)&data[0]) >> 8)
 ;
 break;
 }
 
 for (; i < size; i += 4) {
 CRC->DR = __RBIT(*(uint32_t*)(uintptr_t)&data[i]);
 }
 return __RBIT(CRC->DR) ^ 0xFFFFFFFF;
 }

This is to demonstrate how to

> use consistent padding bytes

I started with one, two or three extra 0xFF, calculated CRC from just them, and then added the "data to change CRC to whatever I want" (and I wanted 0xFFFFFFFF) as per Clive's recipe (last post in that thread). That's how those constants above came to be. The rest is input and output bit reversal as per CCITT-32, and the final xor.

JW