Skip to main content
Gencay
Associate III
Apr 24, 2023 6:27 AM UTC
Solved

STM32CubeU5 TFM Application (UM2581) on U575

Hello,

Can we run STM32CubeU5 TFM Application (UM2581) on U575 since it has not crypto hw like U585?

Thank you in advance!

Best Regards!

This topic has been closed for replies.
Bubbles
BubblesBest answer
ST Employee
Apr 24, 2023 7:00 AM UTC

Hi @Gencay​,

yes, crypto library will also work. TF-M needs the TrustZone isolation hardware, cryptography software implementation is a compromise that is acceptable.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

Bubbles
BubblesBest answer
ST Employee
Apr 24, 2023 7:00 AM UTC

Hi @Gencay​,

yes, crypto library will also work. TF-M needs the TrustZone isolation hardware, cryptography software implementation is a compromise that is acceptable.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Gencay
GencayAuthor
Associate III
Apr 24, 2023 7:09 AM UTC

Hello @JHOUD​ Thank you for your answer.

May I also ask which one does ST suggests? TF-M or X-CUBE-SBSFU?

Thank you in advance!

Best Regards.

Bubbles
ST Employee
Apr 24, 2023 7:40 AM UTC

Hi, I believe X-CUBE-SBSFU package is not really a TFM. But in STM32cubeU5 package there are TFM and SBSFU applications - both for U585, so you need to replace the cryptography with library, but both are basically TF-M. Pick whichever you like more. The one called SBSFU is trying to ease transition from non-TZ SBSFU, like for former STM32L4 users, while the other is cleaner TF-M, but the difference is mostly in the application, not in the loader or boot part.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
Sep 17, 2024 1:51 PM UTC

Hello @Gencay;

I'm working on the same topic: porting TFM Application designed for STM32U585xx to STM32U575xx. Can you please list the steps you follow to get this?

Many thanks in advance