STM32CubeProgrammer Default DA Configuration, TZ Enabled, DA Fails - STM32H563 OEMiROT
- 6 replies
- 1054 views
Hi,
I am trying to get the OEMiROT example projects running on STM32H563 from "STM32CubeH5\Projects\NUCLEO-H563ZI\Applications\ROT". The provision.bat script fails after writing option bytes (probably after enabling TZ) and tries to reconnect to the MCU, which is where the script fails.
To get around this, I am trying to do what "provisioning.bat" does manually. I compiled the "OEMiROT_Boot", "OEMiROT_Appli_TrustZone" apps (secure and non-secure) in STM32CubeIDE and the expected .hex are generated. Here are the steps I followed next in STM32CubeProgrammer:
- Product state set to "Provisioning". At this stage, STM32CubeProgrammer confirms if default DA configuration is to be used. I select yes. Successful.
- Enable TrustZone. Successful.
- Write "OEMiROT_Config.obk". Successful.
- Flash all .bin and .hex compiled in "STM32CubeH5\Projects\NUCLEO-H563ZI\Applications\ROT".
- Set product state to "iROT Provisioned". MCU disconnects, reset problems reported, debugger cannot reconnect.
- I try DA. DA is in Certificate authentication mode, as expected in TZ enabled mode.
- I try to use the "key_3_leaf.pem" and "cert_leaf_chain.b64" provided in "STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\DA_Default_Config\STM32H5". I try Full Regression but it fails - "Debug Authentication failed". I chose the key and certificate from "DA_Default_Config\" as I chose default DA configuration in step 1. Trimmed log attached.
This failure is not letting me continue with the OEMiROT examples and concepts in general. I believe this error has currently nothing to do with the OEMiROT I am trying to run.
Which key/certificate combination should be used when default DA configuration in STM32CubeProgrammer is chosen? Can some combination in "STM32CubeH5\Projects\NUCLEO-H563ZI\ROT_Provisioning\DA" help?