Skip to main content
MSaez.1
Associate II
June 30, 2022
Solved

STM32 cryptografic AES CCM libraries giving wrong results

Hello everyone

I am trying to use the crypto library to perform an AES CCM encryption decryption. I am using an STM32F423CH MCU. The frames I am receiving are comming from other system and the authentication is always failing.

I implemted the validation scheme that appears in the NIST Special Publication 800-38C for CCM.

//FROM THE EXAMPLE IN nvlpubs.nist.gov
 const uint8_t key[] = {0x40, 0x41, 0x42, 0x43, 0x44, 0x45, 0x46, 0x47, 0x48, 0x49, 0x4A, 0x4B, 0x4C, 0x4D, 0x4E, 0x4F};
 uint8_t nonce[] = {0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16};
 uint8_t header[] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07};
 uint8_t data[] = {0x20, 0x21, 0x22, 0x23};
 uint8_t outputData[40];
 uint8_t outputTag[8];
 uint8_t recoveredData[32];
 int32_t outputLength = 4;
 int32_t outputTagLength;
 
 
 volatile uint32_t error_status = AES_SUCCESS;
 AESCCMctx_stt AESCCMctx;
 AESCCMctx_stt* AESctx = &AESCCMctx;
 
	AESctx->mNonceSize = 7;
	AESctx->mKeySize = CRL_AES128_KEY;
	AESctx->mFlags = E_SK_DEFAULT;
	AESctx->mAssDataSize = 8;
	AESctx->mTagSize = 4;
	AESctx->mPayloadSize = 4;
	AESctx->pmTag = outputTag;
 
 
 
	error_status = AES_CCM_Encrypt_Init(AESctx, key, nonce);
 
	error_status = AES_CCM_Header_Append(AESctx, header, 8);
 
	error_status = AES_CCM_Encrypt_Append(AESctx, data, 4, outputData, &outputLength);
 
	error_status = AES_CCM_Encrypt_Finish(AESctx, outputData + 4, &outputTagLength);

I am using the SMALL implementation from the library. The expected output is:

MSG:0x71 0x62 0x01 0x5b

MAC: 0x4d 0xac 0x25 0x5d

But the result I am getting is:

MSG: 0x02 0x20 0x1d 0x49 

MAC: 0x49 0x37 0x36 0xab  

Though the decryption with the same libraries gives a positive result

AESctx->mNonceSize = 7;
	AESctx->mKeySize = CRL_AES128_KEY;
	AESctx->mFlags = E_SK_DEFAULT;
	AESctx->mAssDataSize = 8;
	AESctx->mTagSize = 4;
	AESctx->mPayloadSize = 4;
	AESctx->pmTag = outputData + 4;
 
	error_status = AES_CCM_Decrypt_Init(AESctx, key, nonce);
 
	error_status = AES_CCM_Header_Append(AESctx, header, 8);
 
	error_status = AES_CCM_Decrypt_Append(AESctx, outputData, 4, recoveredData, &outputLength);
 
 
	error_status = AES_CCM_Decrypt_Finish(AESctx, recoveredData, &outputLength);

Error_status = 1003 (SUCCESS) and the message match with the original.

Am I doing something wrong? Using the mbedtls libraries is working fine.

Thank you in advance for any support.

This topic has been closed for replies.
MSaez.1
MSaez.1Best answer
Associate II
July 4, 2022

First problem solved! I did not activate the CRC module before using the firmware version of the Cryptographic Library. Thanks to the video "Security Part3 - STM32 Security features - 30 - Crypto library lab"!

3 replies

MSaez.1
MSaez.1Author
Associate II
July 3, 2022

Something is completly wrong somewhere. I have been doing steps in different location and going to the basics but it is still not working.

I activated the AES HW aceleration module to do the encryption/decryption there. I did not get CCM working but going even further I tried to replicate the example on the STM video tutorial on youtube:

Security Part3 - STM32 Security features - 25 - AES CRYPT lab (I cannot add the link directly).

This video tries to replicate one of the examples of the ECB encryption/decryption of the standard NIST Special Publication 800-38A. I am trying to replicate exactly the same example.

The function HAL_CRYP_Encrypt used in this video is not available in the version of the HAL drivers I am using (V.1.21.0) but i tried using the functions HAL_CRYP_AESECB_Encrypt and HAL_CRYPEx_AES. I even tried using the 32bits and the 8 bits configuration posibilities but none of them gave the expected result:

0693W00000QKKn7QAH.png 

CRYP_HandleTypeDef hcryp;
__ALIGN_BEGIN static const uint8_t pKeyAES[32] __ALIGN_END = {
 0x60,0x3D,0xEB,0x10,0x15,0xCA,0x71,0xBE,0x2B,0x73,
 0xAE,0xF0,0x85,0x7D,0x77,0x81,0x1F,0x35,0x2C,0x07,
 0x3B,0x61,0x08,0xD7,0x2D,0x98,0x10,0xA3,0x09,0x14,
 0xDF,0xF4};
 
CAN_HandleTypeDef hcan1;
 
SPI_HandleTypeDef hspi1;
 
TIM_HandleTypeDef htim1;
 
UART_HandleTypeDef huart1;
DMA_HandleTypeDef hdma_usart1_rx;
DMA_HandleTypeDef hdma_usart1_tx;
 
osThreadId defaultTaskHandle;
 
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
__ALIGN_BEGIN static const uint32_t pKeyAES32b[8] __ALIGN_END = {
 0x603DEB10,0x15CA71BE,0x2B73AEF0,0x857D7781,0x1F352C07,
 0x3B6108D7,0x2D9810A3,0x0914DFF4};
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_TIM1_Init(void);
static void MX_SPI1_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_CAN1_Init(void);
static void MX_AES_Init(void);
void StartDefaultTask(void const * argument);
 
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
 
/* USER CODE END PFP */
 
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 *
 * @retval None
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration----------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_TIM1_Init();
 MX_SPI1_Init();
 MX_USART1_UART_Init();
 MX_CAN1_Init();
 MX_AES_Init();
 /* USER CODE BEGIN 2 */
// Plaintext 6bc1bee22e409f96e93d7e117393172a
// Input Block 6bc1bee22e409f96e93d7e117393172a
// Output Block f3eed1bdb5d2a03c064b5a7e3db181f8
// Ciphertext f3eed1bdb5d2a03c064b5a7e3db181f8
 uint32_t plaintext32b[4] = {0x6bc1bee2, 0x2e409f96, 0xe93d7e11, 0x7393172a};
 uint32_t encryptedData32b[4];
 uint32_t decryptedData32b[4];
 
 uint8_t plaintext[16] = {0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96, 0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a};
 uint8_t encryptedData[16];
 uint8_t decryptedData[16];
 volatile HAL_StatusTypeDef ret;
 ret = HAL_CRYPEx_AES(&hcryp, (uint8_t*)plaintext32b, 4, (uint8_t*)encryptedData32b, 1000);
 
 if (ret != HAL_OK)
	{
	 while(1);
	}
 
 ret = HAL_CRYP_AESECB_Encrypt(&hcryp, (uint8_t*)plaintext32b, 4, (uint8_t*)encryptedData32b, 1000);
 if (ret != HAL_OK)
 	{
 	 while(1);
 	}
 ret = HAL_CRYP_AESECB_Decrypt(&hcryp, (uint8_t*)encryptedData32b, 4, (uint8_t*)decryptedData32b, 1000);
 if (ret != HAL_OK)
 	{
 	 while(1);
 	}
 ret = HAL_CRYP_DeInit(&hcryp);
 
 hcryp.Init.pKey = (uint8_t *)pKeyAES;
 
 if (HAL_CRYP_Init(&hcryp) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 
 ret = HAL_CRYP_AESECB_Encrypt(&hcryp, plaintext, 16, encryptedData, 1000);
 if (ret != HAL_OK)
 	{
 	 while(1);
 	}
 ret = HAL_CRYP_AESECB_Decrypt(&hcryp, encryptedData, 16, decryptedData, 1000);
 if (ret != HAL_OK)
 	{
 	 while(1);
 	}
 
 
 /* USER CODE END 2 */
 
 /* USER CODE BEGIN RTOS_MUTEX */
 /* add mutexes, ... */
 /* USER CODE END RTOS_MUTEX */
 
 /* USER CODE BEGIN RTOS_SEMAPHORES */
 /* add semaphores, ... */
 /* USER CODE END RTOS_SEMAPHORES */
 
 /* USER CODE BEGIN RTOS_TIMERS */
 /* start timers, add new ones, ... */
 /* USER CODE END RTOS_TIMERS */
 
 /* Create the thread(s) */
 /* definition and creation of defaultTask */
 osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);
 defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
 
 /* USER CODE BEGIN RTOS_THREADS */
 /* add threads, ... */
 /* USER CODE END RTOS_THREADS */
 
 /* USER CODE BEGIN RTOS_QUEUES */
 /* add queues, ... */
 /* USER CODE END RTOS_QUEUES */
 
 
 /* Start scheduler */
 osKernelStart();
 
 /* We should never get here as control is now taken by the scheduler */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 
 }
 /* USER CODE END 3 */
 
}

I am starting to think that something it mad in my MCU or in the drivers. Can please someone support!?

Best regards

PS: As commented before using the MBEDTLS SW I got it working straight forward. Regretfully this is too slow for my application. Any advice would be greatly wellcome.

MSaez.1
MSaez.1AuthorBest answer
Associate II
July 4, 2022

First problem solved! I did not activate the CRC module before using the firmware version of the Cryptographic Library. Thanks to the video "Security Part3 - STM32 Security features - 30 - Crypto library lab"!

Tesla DeLorean
Guru
July 8, 2022

This is one of the gotchas with the libraries, this needs to be emphasized in the examples and README file.

And honestly a requirement that needs to be removed, and moved beyond.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..