Skip to main content
Grogu
Associate III
Jun 9, 2022 6:17 AM UTC
Question

SFI : Error: RSS internal system error or License is invalid!

Device details :

ST-LINK SN : 002F003F3137510539383538

ST-LINK FW : V3J9M3B5S1

Board    : STLINK-V3SET

Voltage   : 3.76V

SWD freq  : 24000 KHz

Connect mode: Hot Plug

Reset mode : Software reset

Device ID  : 0x480

Revision ID : --

Device name : STM32H7A/B

Flash size : 2 MBytes

Device type : MCU

Device CPU : Cortex-M7

BL Version : 0x91

When trying to program SFI file to device getting below error

Error: SECURITY State Fail
Error: Invalid state after SFI install !
Error: RSS internal system error or License is invalid !
 

SFI creation :

on0693W00000NrUfRQAV.pngFull logs:

./STM32_Programmer_CLI -c port=swd mode=HOTPLUG -sfi protocol=static /home/analog/drive/SFIFiles/sbsfu_rdp_bb.sfi hsm=1 slot=1
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.10.0 
 -------------------------------------------------------------------
 
ST-LINK SN : 002F003F3137510539383538
ST-LINK FW : V3J9M3B5S1
Board : STLINK-V3SET
Voltage : 3.76V
SWD freq : 24000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x480
Revision ID : --
Device name : STM32H7A/B
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x91
 
 Protocol Information : static
 
 SFI File Information : 
 
 SFI file path : /home/analog/drive/SFIFiles/sbsfu_rdp_bb.sfi
 SFI HSM slot ID : 1
 SFI header information : 
 SFI protocol version : 2
 SFI total number of areas : 9
 SFI image version : 2
 SFI Areas information : 
 
 Parsing Area 1/9 : 
 Area type : F
 Area size : 688
 Area destination address : 0x8000000
 
 Parsing Area 2/9 : 
 Area type : F
 Area size : 20400
 Area destination address : 0x8000400
 
 Parsing Area 3/9 : 
 Area type : F
 Area size : 2704
 Area destination address : 0x8006000
 
 Parsing Area 4/9 : 
 Area type : F
 Area size : 176
 Area destination address : 0x8007000
 
 Parsing Area 5/9 : 
 Area type : F
 Area size : 72848
 Area destination address : 0x8007100
 
 Parsing Area 6/9 : 
 Area type : P
 Area size : 32
 Area destination address : 0x81ff000
 
 Parsing Area 7/9 : 
 Area type : R
 Area size : 32
 Area destination address : 0x81ff000
 
 Parsing Area 8/9 : 
 Area type : F
 Area size : 29024
 Area destination address : 0x8028000
 
 Parsing Area 9/9 : 
 Area type : C
 Area size : 36
 Area destination address : 0x0
 
Reading the chip Certificate...
 
 
Requesting Chip Certificate from device ...
 
Get Certificate done successfully
 
requesting license for the current STM32 device
 
Init Communication ...
 
ldm_LoadModule(): loading module "./libstp11_SAM.so" ... 
ldm_LoadModule: OK loading library "./libstp11_SAM.so": 0x018ED970 ... 
C_GetFunctionList() returned 0x00000000, g_pFunctionList=0x5F696060
P11 lib initialization Success!
 
Opening session with solt ID 1...
 
Succeed to Open session with reader solt ID 1
 
Succeed to generate license for the current STM32 device
 
Closing session with reader slot ID 1...
 
Session closed with reader slot ID 1
 
Closing communication with HSM...
 
Communication closed with HSM
 
Succeed to get License for Firmware from HSM slot ID 1
 
Starting Firmware Install operation...
 
 
Activating security...
Warning: Option Byte: SECURITY, value: 0x1, was not modified.
Warning: Option Bytes are unchanged, Data won't be downloaded
Time elapsed during option Bytes configuration: 00:00:00.002
Activating security Success
Setting write mode to SFI
Warning: Option Byte: SECURITY, value: 0x1, was not modified.
Warning: Option Byte: ST_RAM_SIZE, value: 0x3, was not modified.
Warning: Option Bytes are unchanged, Data won't be downloaded
Time elapsed during option Bytes configuration: 00:00:00.002
Succeed to set write mode for SFI
 
Starting SFI part 1
 
Writing license to address 0x24020800
Writing Img header to address 0x24021000
Writing areas and areas wrapper...
RSS process started...
 
RSS command execution OK
RSS complete Value = 0x16
Reconnecting...
ST-LINK SN : 002F003F3137510539383538
ST-LINK FW : V3J9M3B5S1
Board : STLINK-V3SET
Voltage : 3.76V
SWD freq : 24000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x480
Revision ID : --
Reconnected !
 
 
Error: SECURITY State Fail
Error: Invalid state after SFI install !
Error: RSS internal system error or License is invalid !
 
Aborting...
Time elapsed during option Bytes configuration: 00:00:00.019
Time elapsed during option Bytes configuration: 00:00:00.028
 
Waiting 8s for end of regression...
Display OB after Abort for sanity check
 
 
OPTION BYTES BANK: 0
 
 Read Out Protection:
 
 RDP : 0xAA (Level 0, no protection) 
 
 BOR Level:
 
 BOR_LEV : 0x0 (reset level OFF) 
 
 User Configuration:
 
 IWDG1_SW : 0x1 (Independent watchdog is controlled by software) 
 NRST_STOP : 0x1 (STOP mode on Domain 1 is entering without reset) 
 NRST_STBY : 0x1 (STANDBY mode on Domain 1 is entering without reset) 
 VDDMMC_HSLV : 0x0 (I/O speed optimization at low-voltage disabled) 
 IWDG_FZ_STOP : 0x1 (Independent watchdog is running in STOP mode) 
 IWDG_FZ_SDBY : 0x1 (Independent watchdog is running in STANDBY mode) 
 SECURITY : 0x1 (Security feature enabled) 
 VDDIO_HSLV : 0x0 (Product working in the full voltage range,I/O speed optimization at low-voltage disabled) 
 SWAP_BANK_OPT: 0x0 (after boot loading, no swap for user sectors) 
 
 Boot address Option Bytes:
 
 BOOT_CM7_ADD0: 0x800 (0x8000000) 
 BOOT_CM7_ADD1: 0x1FF0 (0x1FF00000) 
 
 PCROP Protection:
 
 PROT_AREA_START1: 0x777 (0x8077700) 
 PROT_AREA_END1: 0x0 (0x80000FF) 
 DMEP1 : 0x1 (Flash Bank 1 PCROP zone is erased when RDP level regression (change from level 1 to 0) occurs) 
 PROT_AREA_START2: 0x777 (0x8177700) 
 PROT_AREA_END2: 0x0 (0x81000FF) 
 DMEP2 : 0x1 (Flash Bank 2 PCROP zone is erased when RDP level regression (change from level 1 to 0) occurs) 
 
 Secure Protection:
 
 SEC_AREA_START1: 0x777 (0x8077700) 
 SEC_AREA_END1: 0x0 (0x80000FF) 
 DMES1 : 0x1 (Flash Bank 1 secure area is erased when RDP level regression (change from level 1 to 0) occurs) 
 SEC_AREA_START2: 0x777 (0x8177700) 
 SEC_AREA_END2: 0x0 (0x81000FF) 
 DMES2 : 0x1 (Flash Bank 2 secure area is erased when RDP level regression (change from level 1 to 0) occurs) 
 
 DTCM RAM Protection:
 
 ST_RAM_SIZE : 0x3 (16 KB) 
 
 Write Protection:
 
 nWRP0 : 0x1 (Write protection not active) 
 ...
 nWRP63 : 0x1 (Write protection not active) 
Abort SUCCESS
 
Error: /home/analog/drive/SFIFiles/sbsfu_rdp_bb.sfi SFI file Install Operation Failure! Please, try again

This topic has been closed for replies.

5 replies

Chloe Meunier
ST Employee
Jun 10, 2022 1:19 PM UTC

Hello,

the problem comes from the compability of SFI with your board . STM32H7A/B are not yet compatible with SFI.

The STM32H7A3xI/G, STM32H7B0xB and STM32H7B3xI device errata mention this incompability paragraph 2.2.3.

https://www.st.com/resource/en/errata_sheet/es0478-stm32h7a3xig-stm32h7b0xb-and-stm32h7b3xi-device-errata-stmicroelectronics.pdf

BR

Chloé

Grogu
GroguAuthor
Associate III
Jun 10, 2022 1:59 PM UTC

Thanks Chloé

​

​For pointing me to compatibility page. What you suggest the direction forward, is there a workaround to program this files on device.

​

​

​

Grogu
GroguAuthor
Associate III
Jun 14, 2022 10:14 PM UTC

@Chloe Meunier​ 

Also CC @Jocelyn RICARD​  @Fred​ ​ 

I tried on dev kit able to program SFI on STM32H7B3I-DK it seems to work which has a Bootloader version 0x90. 0693W00000NrrKvQAJ.png 

I am a bit confused now with

The STM32H7A3xI/G, STM32H7B0xB and STM32H7B3xI device errata mention this incompatibility paragraph 2.2.3.

https://www.st.com/resource/en/errata_sheet/es0478-stm32h7a3xig-stm32h7b0xb-and-stm32h7b3xi-device-errata-stmicroelectronics.pdf

What is not supported/partially compatible?

PROGRAMMING OPTION BYTES AREA ...
Database: Config 0 is active.
Warning: Option Byte: SECURITY, value: 0x1, was not modified.
Warning: Option Byte: ST_RAM_SIZE, value: 0x3, was not modified.
 
Warning: Option Bytes are unchanged, Data won't be downloaded
Time elapsed during option Bytes configuration: 00:00:00.005
Succeed to set write mode for SFI
 
Starting SFI part 1
 
Writing license to address 0x24020800
Writing Img header to address 0x24021000
Writing areas and areas wrapper...
all areas processed
RSS process started...
 
halt ap 0
run ap 0
RSS command execution OK
Warning: Could not verify security state after last chunk programming
SFI Process Finished!
SFI file c:/drive/sfifiles/sbsfu_bb.sfi Install Operation Success
 
Time elapsed during SFI install operation: 00:00:01.528
Disconnected

Looks like this is been fixed on BL version 9.2 and RSS 3.1.0 for revision X. However my dev board has BL version 9.0

0693W00000NrwDkQAJ.pngHoping to get a bit more insights about the errata few features of SFI not supported or SFI as a whole.

TIA

Jocelyn RICARD
ST Employee
Jun 29, 2022 11:55 AM UTC

Hello @Community member​ ,

You can experiment SFI at development stage with your bootloader version but it will not be 100% reliable. You may see some corrupted data in flash.

Also, new version should improve flashing speed.

Best regards

Jocelyn

Grogu
GroguAuthor
Associate III
Jul 1, 2022 4:13 PM UTC

@Jocelyn RICARD​  thanks,

As this is part of the STM system bootloader which we can't change I assume. what would you suggest moving to a different SKU of H7?.