Skip to main content
Mr_M_from_G
Senior II
May 24, 2024
Solved

Searching counterpart for STM32CubeExpansion_Crypto_V4.2.0 ECDSA

I implemented a ECDSA signature generation and checking on STM32H743ZI NUCLEO using STM32CubeExpansion_Crypto_V4.2.0 library example ECDSA_SignVerify.

I did similiar with Python using https://pypi.org/project/ecdsa/

Unfortunately signature generated by one fail to verify with the other although using the same input for hash, private and public key and curve. I used SECP256k1 / SECP256K1 and NIST256p / SECP256R1 on Python / STM32.

Any suggestions? What are the tools ST verified the libraries with?

Verification on the same platform works fine in both cases.

Thanks for any help.

 

 

This topic has been closed for replies.
Mr_M_from_G
Mr_M_from_GBest answer
Senior II
June 20, 2024

Python's ecdsa function verify always does a hash internally, I needed to use verify_digest.

2 replies

Tesla DeLorean
Guru
May 24, 2024

I used patterns here for SECP256K1

https://github.com/pyca/cryptography/blob/main/vectors/cryptography_vectors/asymmetric/ECDSA/SECP256K1/SigGen.txt#L6314

Using a early version of Easy ECC, something I can build readily with MSVC, KEIL and GNU/GCC without a complete circus. I have to address some endian issues, but I understand them..

For the  SECP192R1 / SECP256R1 I used NIST's materials directly, ie FIPS 186-2 and/or FIPS 186-4

https://csrc.nist.gov/projects/cryptographic-algorithm-validation-program/digital-signatures#ecdsa2vs

Using  SigGen.txt [P-256,SHA-256] test vectors

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Mr_M_from_G
Mr_M_from_GAuthorBest answer
Senior II
June 20, 2024

Python's ecdsa function verify always does a hash internally, I needed to use verify_digest.