Skip to main content
APara.5
Associate II
Jun 7, 2021 10:01 PM UTC
Question

SBSFU software - STM32L476RG_NUCLEO_2_Images_UserApp not building error :

[9568] Failed to execute script prepareimage

Traceback (most recent call last):

 File "prepareimage.py", line 861, in <module>

 File "prepareimage.py", line 858, in args

 File "prepareimage.py", line 124, in do_encrypt

 File "keys.py", line 262, in load

FileNotFoundError: [Errno 2] No such file or directory: '../../../../2_Images_SECoreBin/SW4STM32/../Binary/OEM_KEY_COMPANY1_key_AES_CBC.bin'

../../../../2_Images_SECoreBin/SW4STM32/postbuild.sh: line 70: prepareimage.exe: No error

prepareimage.exe enc -k ../../../../2_Images_SECoreBin/SW4STM32/../Binary/OEM_KEY_COMPANY1_key_AES_CBC.bin -i ../../../../2_Images_SECoreBin/SW4STM32/../Binary/iv.bin ../../UserApp.bin ../../../Binary/UserApp.sfu : failed

make[1]: *** [makefile:97: post-build] Error 1

make: *** [makefile:63: all] Error 2

"make -j8 all" terminated with exit code 2. Build might be incomplete.

Im not sure what the issue is- I haven't modified any of the code- just tried to rebuild the project using STM32CubeIDE

This topic has been closed for replies.

2 replies

Bubbles
ST Employee
Jun 8, 2021 6:56 AM UTC

Hello @APara.5​ ,

looks like you placed the project too deep into the directory system.

Try moving it to a directory with shorter path, closer to the root directory, like for example "C:\SBSFU\".

Let me know if that helped

Rgds,

Jarda

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
APara.5
APara.5Author
Associate II
Jun 8, 2021 5:10 PM UTC

That worked, thank you!