Skip to main content
Associate II
Nov 12, 2024 2:20 PM UTC
Question

SBSFU not detecting Active Slot Image

I'm working on integrating the latest SBSFU (v2.6.2) onto an STM32L4A6 platform. I've reviewed both the user manual and application note for the SBSFU, as well as the examples provided.

In my use case:

  • I have an external attached MMC flash
  • I'm not planning to use the internal MCU flash dual-bank capability (so I can have an image larger than half the 1MB flash size)
  • I don't need rollback/swap capability
  • For OTA updates, my user application will download the encrypted image to a location in the external MMC flash. The SBSFU on boot will check for a valid image in that location, and if so, it will copy it to the MCU flash active slot.

 

I was able to get the B-L475E-IOT01A 2_Images_ExtFlash example to boot and run on my board, and it executes the UserApp.

 

For porting the SBSFU to integrate with my custom UserApp I have:

  • Started from the B-L475E-IOT01A 2_Images_ExtFlash example because it seemed like the closest for what I needed.
  • Replaced the example QSPI driver with an MMC flash driver
  • Modified the various linker files how I think they should be modified based on the user manual/app note.
  • Temporarily disabled all security protections in the SBSFU and enabled verbose debugging
  • The example I started from with external flash was putting the FIREWALL NVDATA section in the middle of the MCU flash (0x8080000) as if we were using dual-bank internal flash, so I changed that by referencing the NUCLEO-L432KC 1_Image example which uses the Firewall but places the NVDATA section at the start of the first active slot (0x8020000).
  • I'm able to build the SECoreBin, SBSFU, and custom UserApp successfuly.
  • When I try to use STMCubeProgrammer to flash the resulting combined binary in to the MCU, it loads but it fails to detect a valid image in Active Slot 1 (the master slot), and then it erases that slot because no valid image was found.
  • I'm having trouble figuring out why it's not seeing a valid image in that location, since it should be part of the combined binary produced by the SBSFU scripts.
    • I've added some trace statements to the when SFU_IMG_DetectFW() is called and more specifically for the SFU_LL_FLASH_INT_Read() function.
    • I can see that when it's searching inside the header region, the se_status returns SE_KO, and the se_ret_status returns SE_ERROR, but I'm not sure how to troubleshoot this further.
    • Here's a console output from some trace logging I've added in this region:

 

SFU_IMG_DetectFW -> slot 1
SFU_LL_FLASH_Read internal
Looking in header
pSource: 0x0x8020000, Length: 320 -> pdest: 0x0x20017e78
DoubleECC_Error_Counter: 0
se_status: 1245757
se_ret_status: 100249
SFU_IMG_DetectFW -> slot 1
SFU_LL_FLASH_Read internal
Looking in header
pSource: 0x0x8020000, Length: 320 -> pdest: 0x0x20017e78
DoubleECC_Error_Counter: 0
se_status: 1245757
se_ret_status: 100249
Slot SLOT_ACTIVE_1 not empty : erasing ...

 

Trying to figure out what my next steps should be to determine why the SBSFU is not finding a valid image in active slot 1.

 

Thanks!

This topic has been closed for replies.

15 replies

Jocelyn RICARD
ST Employee
Nov 13, 2024 1:11 PM UTC

Hello @jmcoreymv ,

I don't fully catch what you have done with NVDATA of firewall.

Just be aware that there is a firewall limitation that you can check in errata sheet that impacts the possible mapping solutions.

In any case, my advice will be to debug the modified SBSFU and try to understand what happens.

You can always add SECoreBin symbols to debug inside SECoreBin. Just make sure to disable firewall and once you make it work, re-enable firewall to see if you don't fall in the limitation.

Best regards

Jocelyn

jmcoreymvAuthor
Associate II
Nov 13, 2024 10:55 PM UTC

I'm going to work a bit more on trying to load the SECoreBin symbols to debug that further.  Currently all SBSFU protections are disabled.

Regarding the firewall limitation, could you help me understand this better for my use-case?  I have the STM32L4A6, but I don't want to use the dual-bank capability since it will limit my potential image size to a bit under half of the 1MB flash.  Instead I'm using the external MMC flash as my download slot, and giving up swap/rollback capabilities.

Is this still possible to do?  So firewall would be enabled, code and NV data would be protected, but I don't want to place NVDATA in the middle of the MCU flash because that would prevent me from supporting larger images.  Is my understanding correct?

Jocelyn RICARD
ST Employee
Nov 14, 2024 6:03 PM UTC

Hello @jmcoreymv ,

the X-CUBE-SBSFU does not use the dual bank capability for update. I mean, the update does not happen using a bank swapping. Update mechanism uses a sector swapping mechanism using a spare sector for robustness in case of reset during the swapping.

The usage of NVData on second bank is used to protect the content of firewall on first bank. Reason is that firewall content moves with bank swapping. So, if you don't have this NVData area on second bank, the firewall content can be exposed. If you remove this, you introduce a weakness. Now, to exploit such weakness an attacker would need to be able to inject code on your target, which is not that easy.

This constraint is described in AN5056 Rev8 Chapter 3.2.2

The risk is to leak the authentication public key and the encryption key.

Authentication public key does not provide any information. Encryption key allows decrypting content of the firmware. So, if attacker manages to inject code, firmware content (outside firewall) has already leaked...

So, risk could be related to what you add inside firewall. Up to you to evaluate the global risk.

Best regards

Jocelyn