Skip to main content
STsch.1
Associate III
Dec 29, 2021 10:42 AM UTC
Question

SBSFU example for the STM32F722

Hi,

I have trouble adapting the STM32F769I_Discovery_2_Images_SBSFU example for the STM32F722. There are so much inconsistencies and I don't really know what I should let out and what really is necessary. For example, the STM32F769I uses somehow the stm32f7xx_hal_flash_ex.h, which is not used by the STM32F722 etc.

Is there a built project available for the STM32F722?

Edit: I could solve all the problems, it was because of the dual bank used in the STM32F769I example

This topic has been closed for replies.

1 reply

Bubbles
ST Employee
Jan 3, 2022 5:12 PM UTC

Hi @STsch.1​ ,

the F722 has much smaller Flash memory, are you sure 2-image is practical in your case?

anyway good luck.

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.