Skip to main content
Associate III
Jan 24, 2024 2:29 PM UTC
Question

SBSFU | B-L4S5I-IOT01A | Build error | Missing function definitions

Hello all,

I'm trying to build B-L4S5I-IOT01A, 2 Images KMS project and I'm encountering the build issue related with missing function definition for KMS_LL_Finalize(). Build fails during linkage phase.

JakubStandarski_0-1706106424035.png

Is that issue related with the wrong version of KMS package provided with SBSFU 2.6.2?

 

PS. Same issue applies for B-L475E-IOT01A project.

This topic has been closed for replies.

4 replies

Jocelyn RICARD
ST Employee
Jan 24, 2024 3:08 PM UTC

Hello Jakub,

yes, this is that issue.

Just get KMS middleware from SBSFU 2.6.1 and copy it in SBSFU 2.6.2 it will solve the issue

Best regards

Jocelyn

 

Bubbles
ST Employee
Jan 24, 2024 3:25 PM UTC

Hello @Jakub Standarski,

what tool did you use to build the project? There is apparently some sort of regression when using newer tool. I encountered same problem using EWARM 9.40, while in EWARM 9.30 it built correctly.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
Jan 24, 2024 3:30 PM UTC

STM32CubeIDE 1.12.1.

I've checked code and definition for the function mentioned above doesn't exist.
I will try KMS version provided by SBSFU 2.6.1 as mentioned by @Jocelyn RICARD .

Thank you for you help!

Bubbles
ST Employee
Sep 26, 2024 7:06 AM UTC

Hi @Jakub Standarski ,

problem is reported fixed in version 2.7.0.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.