Skip to main content
sute
Associate III
Nov 30, 2021 3:55 PM UTC
Question

SBSFU and userApp bigelf size

Hello,

I am trying to generate the combined elf file with SBSFU and user app. The provided postbuild scripts use the following code to create the file:

command=$programmertool" -ms "$elf" "$headerbin" "$sbsfuelf

There is a problem that the combined elf file is huge. For my own application it is 147M and for the example userApp 59M. Why is the file so big? How do I get a normal combination elf file? The combination bin-file is normal and works.

    This topic has been closed for replies.

    5 replies

    Jocelyn RICARD
    ST Employee
    Nov 30, 2021 5:58 PM UTC

    Hello @MS.12utela​ 

    I checked on simple STM32L476 example on last SBSFU 2.5.0 and I get 23M elf file.

    Looking inside, it is full of zeros. I don't know why.

    STM32CubeIDE provides elf tools in (for CubeIDE 1.8.0)

    plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\bin\

    arm-none-eabi-readelf.exe UserApp.elf  shows a very big section .shstrtab

    Then, I tried using command

    arm-none-eabi-objcopy.exe --strip-unneeded UserApp.elf

    elf size is now 78 KB

    Now, I'm not sure this combined elf feature is well tested in SBSFU.

    What are you trying to do with it ?

    Best regards

    Jocelyn

    sute
    suteAuthor
    Associate III
    Dec 1, 2021 4:36 PM UTC

    Hi thanks for help!

    I am trying to get an elf file that I can debug on the MCU.

    Indeed, running arm-none-eabi-objcopy on my own application I am able to decrease the elf size, however I get two warnings:

    st4M9tlx: section .isr_vector lma 0x8010034 adjusted to 0x8018400

    st4M9tlx: warning: allocated section `Header' not in segment

    The first one seems OK, but not the second one. I am also unable to run the elf file on target.

    Jocelyn RICARD
    ST Employee
    Dec 1, 2021 5:53 PM UTC

    Hello @MS.12utela​ 

    OK so in order to debug I would suggest doing the following:

    1) Flash the big binary generated

    2) setup your debugger to only load symbols: You can load symbols of SBSFU, SE and application with associated elf files (deactivate generation with programmer)

    3) Attach to target and debug

    Best regards

    Jocelyn

    sute
    suteAuthor
    Associate III
    Dec 2, 2021 3:20 PM UTC

    Thanks. I have been debugging and it seems to me that STM32_Programmer_CLI places the Header section to wrong place. Here are the section headers using arm-none-eabi-readelf from combined bootloader and userApp elf file from the SBSFU examples:

    Section Headers: [Nr] Name Type Addr Off Size ES Flg Lk Inf Al [ 0] NULL 00000000 000000 000000 00 0 0 0 [ 1] .isr_vector PROGBITS 08018400 0001b4 000400 00 A 0 0 1 [ 2] .text PROGBITS 08018800 00f47c 0052d8 00 AX 0 0 16 [ 3] .rodata PROGBITS 0801dad8 014754 000f40 00 A 0 0 4 [ 4] .ARM.extab PROGBITS 0801ea18 015b3c 000000 00 W 0 0 1 [ 5] .ARM ARM_EXIDX 0801ea18 015694 000008 00 AL 2 0 4 [ 6] .preinit_array PREINIT_ARRAY 0801ea20 01569c 000000 04 WA 0 0 1 [ 7] .init_array INIT_ARRAY 0801ea20 01569c 000008 04 WA 0 0 4 [ 8] .fini_array FINI_ARRAY 0801ea28 0156a4 000008 04 WA 0 0 4 [ 9] .data PROGBITS 20001000 0156ac 000078 00 WA 0 0 4 [10] .align32 PROGBITS 0801eaa8 015724 000018 00 WA 0 0 1 [11] .bss NOBITS 20001078 015b3c 0005ac 00 WA 0 0 4 [12] ._user_heap_stack NOBITS 20001624 015b3c 000a04 00 WA 0 0 1 [13] .ARM.attributes ARM_ATTRIBUTES 00000000 015b3c 00002e 00 0 0 1 [14] .comment PROGBITS 00000000 015b6a 000053 01 MS 0 0 1 [15] SBSFU0 PROGBITS 08000000 0005b4 0002b0 00 WA 0 0 4 [16] SBSFU1 PROGBITS 08000404 000864 005154 00 WA 0 0 4 [17] SBSFU2 PROGBITS 08006000 0059b8 0007cc 00 WA 0 0 4 [18] SBSFU3 PROGBITS 08006900 006184 000088 00 WA 0 0 4 [19] SBSFU4 PROGBITS 08006a00 00620c 009270 00 WA 0 0 4 [20] Header PROGBITS 20000c78 01573c 000400 00 WA 0 0 4 [21] .shstrtab STRTAB 00000000 015bbd 0000c5 00 0 0 1

    Note that the address for Header is 0x20000c78 while it should be 0x0801800 according to mapping_fwimg.ld. Is this a bug or am I doing something wrong?

    Is there a simple way to fix this?

    Jocelyn RICARD
    ST Employee
    Dec 2, 2021 3:51 PM UTC

    Hello @MS.12utela​ 

    As I said, I'm not sure this feature is working well.

    So, to debug please use original elf files generated by the compiler.

    Best regards

    Jocelyn