Skip to main content
Associate II
February 29, 2024
Solved

Regenerating OEMiRoT_Data.obk

Hi,

While using the STM32Cube_FW_H5_V1.1.1 repository to explore secure boot on the STM32H5, I saw that the configuration file to generate OEMiRoT_Data.obk is missing. As I want to use my own keys and certificates for the OEMiRoT example application, I think I should regenerate the OEMiRoT_Data.obk file, but I can't find how to do this.

Am i missing something, or is the OEMiRoT_Data.xml file missing from the repository?

Best,

Jens

This topic has been closed for replies.
Frantz LEFRERE
Frantz LEFREREBest answer
ST Technical Moderator
March 1, 2024

Hi @jens-vdb 

in fact we do not provide an xml to generate this OEMiRoT_Data.obk.
As this one is only initialize data region used by OEM-iRot to 0, you don't need to tune it.

Basically the obk syntax is 
Address / Size /  Flag / SHA256 ( content)  / Content
If you dump the content you will find the sha256 : 
0x B3 93 97 88 42 A0 FA 3D 3E 14 70 19 6F 09 8F 47 3F 96 78 E7 24 63 CB 65 EC 4A B5 58 18 56 C2 E4

Data Content 
0x00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000

So you can use it as it's.

Best regards,

Frantz 

4 replies

ST Technical Moderator
February 29, 2024

Hello @jens-vdb ,

I advise you follow this wiki page How to start with OEMiRoT on STM32H573 and 563–Arm® TrustZone® enabled - stm32mcu to generate a customized configuration file.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
jens-vdbAuthor
Associate II
February 29, 2024

Hi @Imen.D ,

On that page I have found instructions to generate the OEMiRoT_Config.obk file (and generate a OEMiRoT_Config.xml) file using the Trusted Package Creator, but that page does not mention anything about the OEMiRoT_Data.obk file and how to generate that.

In the repository both the OEMiRoT_Config.obk and OEMiRoT_Config.xml files are present, but only OEMiRoT_Data.obk and *not* OEMiRoT_Data.xml. It is that last xml file that I don't know what to put in there.

Frantz LEFRERE
Frantz LEFREREBest answer
ST Technical Moderator
March 1, 2024

Hi @jens-vdb 

in fact we do not provide an xml to generate this OEMiRoT_Data.obk.
As this one is only initialize data region used by OEM-iRot to 0, you don't need to tune it.

Basically the obk syntax is 
Address / Size /  Flag / SHA256 ( content)  / Content
If you dump the content you will find the sha256 : 
0x B3 93 97 88 42 A0 FA 3D 3E 14 70 19 6F 09 8F 47 3F 96 78 E7 24 63 CB 65 EC 4A B5 58 18 56 C2 E4

Data Content 
0x00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000

So you can use it as it's.

Best regards,

Frantz