Skip to main content
Associate
Nov 8, 2024 7:39 AM UTC
Question

Public Key decompression, get Y from X: HAL_PKA_ModExp wrong output

Hello,

I have implemented most of the functions required for decompressing the public key using the PKA arithmetic functions. But, I'm encountering a timeout error with HAL_PKA_ModExp, even when setting a high delay with HAL_MAX_DELAY. Additionally, the output data is incorrect. Here is a simplified version of my code:
uint8_t data[96] = {
0x9c, 0x29, 0xec, 0x4b, 0xd7, 0x69, 0xf4, 0xe9, 0x30, 0xc7, 0xb0, 0x14, 0x2e, 0x51, 0x81, 0xff,
0x98, 0x8c, 0xb1, 0xa0, 0x3e, 0x66, 0xf8, 0xcc, 0x62, 0x13, 0xb5, 0xed, 0xf6, 0x89, 0xfc, 0x9d,
0x37, 0x0e, 0xa0, 0x94, 0xfe, 0x9e, 0x8d, 0xd5, 0x64, 0xf9, 0x05, 0x28, 0x22, 0x42, 0xfd, 0x87,
0xec, 0xb2, 0x99, 0x5c, 0xaf, 0x3c, 0x0d, 0x9d, 0xd7, 0xcf, 0x2f, 0x35, 0xda, 0xf0, 0xcb, 0xc7,
0xb8, 0xcd, 0x7c, 0xc1, 0xe0, 0xed, 0xa6, 0x13, 0xe5, 0xbd, 0x07, 0xfb, 0x81, 0x80, 0xb6, 0x4a,
0x1a, 0x27, 0x80, 0xd9, 0xd8, 0xc5, 0x28, 0xa0, 0xae, 0xe2, 0xb2, 0xef, 0x93, 0x37, 0x91, 0xa3
};

uint8_t exponent[32] = {
0x3f, 0xff, 0xff, 0xff, 0xc0, 0x00, 0x00, 0x00, 0x40, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x40, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
};

uint8_t mod[96] = {
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0xff, 0xff, 0xff, 0xff, 0x00, 0x00, 0x00, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff
};

PKA_ModExpInTypeDef sModExpConfig;
sModExpConfig.expSize = 32;
sModExpConfig.OpSize = 96;
sModExpConfig.pExp = exponent;
sModExpConfig.pOp1 = data;
sModExpConfig.pMod = mod;

uint8_t resultModExp[100];
memset(resultModExp, 0, 100);

if (HAL_PKA_ModExp(&hpka, &sModExpConfig, 10000) != HAL_OK) {
printf("Modular exponentiation timed out.\n");
}

HAL_PKA_ModExp_GetResult(&hpka, resultModExp);

The expected result is (calculated using python):
plaintext = 0x9c29ec4bd769f4e930c7b0142e5181ff988cb1a03e66f8cc6213b5edf689fc9d370ea094fe9e8dd564f905282242fd87ecb2995caf3c0d9dd7cf2f35daf0cbc7b8cd7cc1e0eda613e5bd07fb8180b64a1a2780d9d8c528a0aee2b2ef933791a3
publicExponent = 0x3fffffffc0000000400000000000000000000000400000000000000000000000
modulus = 0x00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000ffffffff00000001000000000000000000000000ffffffffffffffffffffffff

result = pow(plaintext, publicExponent, modulus)
print("Mod Exp: ")
print(hex(result))

--> 0x80d6d17eb470e9b87827860307fbd48b4adef1ad9346527a32cd6e34e64e7ec2


But, Strangely, HAL_PKA_ModExp works as expected with a different modulus and exponent setup:

uint8_t modulus[96] = {
0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25,
0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25,
0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25,
0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25,
0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25,
0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25, 0x23, 0x22, 0x22, 0x25};

uint8_t publicExponent[32] = {
0x00, 0x00, 0x05, 0x01, 0x00, 0x00, 0x05, 0x01, 0x00, 0x00, 0x05, 0x01, 0x00, 0x00, 0x05, 0x01,
0x00, 0x00, 0x05, 0x01, 0x00, 0x00, 0x05, 0x01, 0x00, 0x00, 0x05, 0x01, 0x00, 0x00, 0x05, 0x01};
};

uint8_t plaintext[96] = {
0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43,
0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43,
0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43,
0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43,
0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43,
0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x43, 0x44, 0x44, 0x44, 0x44};
};

expected result:
plaintext = 0x444444434444444344444443444444434444444344444443444444434444444344444443444444434444444344444443444444434444444344444443444444434444444344444443444444434444444344444443444444434444444344444444
publicExponent = 0x0000050100000501000005010000050100000501000005010000050100000501
modulus = 0x232222252322222523222225232222252322222523222225232222252322222523222225232222252322222523222225232222252322222523222225232222252322222523222225232222252322222523222225232222252322222523222225
result = pow(plaintext, publicExponent, modulus)
print("Mod Exp: ")
print(hex(result))
--> 0xeac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac92680eac9269

 

Could you please help me to find out the problem ?Has anyone encountered a similar issue with HAL_PKA_ModExp? Are there specific constraints on modulus or exponent values that could cause this behavior? Any advice on potential fixes or workarounds would be greatly appreciated!

This topic has been closed for replies.