Skip to main content
Associate III
May 27, 2024
Solved

OPTSR_PRG flash register not updating after enabling secure user memory

Hello everyone,

i am trying to enable the secure user memory on the stm32h743 using the x-cube-sbsfu project and have the following problem:
After activating the security bit, the value of the OPTSR_PRG flash register is not changing, so the security bit is not set and therefore i cannot configure the secure user memory.

I use the function SFU_LL_SECU_SetProtectionSecUser from the sfu_low_level_security.c file for the configuration and before calling the function i also called HAL_FLASH_Unlock() and HAL_FLASH_OB_Unlock().

Does anyone know what could be the problem?

 

 

/**
 * @brief Apply Secure User Memory protection.
 * psFlashOptionBytes: pointer to the Option Bytes structure.
 * pbIsProtectionToBeApplied: Output parameter to be set as "TRUE" if
 * this OptByte has to be modified and immediately reloaded.
 * @retval SFU_ErrorStatus SFU_SUCCESS if successful, SFU_ERROR otherwise.
 */
SFU_ErrorStatus SFU_LL_SECU_SetProtectionSecUser(FLASH_OBProgramInitTypeDef *psFlashOptionBytes,
 SFU_BoolTypeDef *pbIsProtectionToBeApplied)
{
 SFU_ErrorStatus e_ret_status = SFU_ERROR;
 SFU_LL_RSS_SecureArea_t aSecureAreas[SFU_LL_RSS_NB_SECURE_AREAS];

 /* Check if Secure User Memory is already configured */
 if (SFU_LL_SECU_CheckProtectionSecUser(psFlashOptionBytes) == SFU_SUCCESS)
 {
 e_ret_status = SFU_SUCCESS;
 }
 else
 {
 /* Apply the proper configuration if we are in development mode */
#if defined(SECBOOT_OB_DEV_MODE)
 /* Set the security bit if needed */
 /* ------------------------------ */
 if ((psFlashOptionBytes->USERConfig & FLASH_OPTSR_SECURITY) == RESET)
 {
 psFlashOptionBytes->Banks = FLASH_BANK_1;
 psFlashOptionBytes->OptionType = OPTIONBYTE_USER;
 psFlashOptionBytes->USERType = OB_USER_SECURITY;
 psFlashOptionBytes->USERConfig = OB_SECURITY_ENABLE;

 if (HAL_FLASHEx_OBProgram(psFlashOptionBytes) == HAL_OK)
 {
 TRACE("\r\n\t Security bit set.");
 /*
 * We need to reload the OBs before configuring the secure user memory area,
 * otherwise the configuration is skipped because Secure Mode is not entered at reset (not booting in RSS).
 *
 * Note: updating pbIsProtectionToBeApplied and e_ret_status would be useless here.
 */
 HAL_FLASH_OB_Launch();
 }
 else
 {
#if defined(SFU_VERBOSE_DEBUG_MODE)
 TRACE("\r\n\t Cannot set the security bit - ERROR");
#endif /* SFU_VERBOSE_DEBUG_MODE */
 return (SFU_ERROR);
 }
 }
 /* else only the secure user memory area needs to be set */

 /* Set the secure user memory area */
 /* ------------------------------- */
 aSecureAreas[0].sizeInBytes = SFU_SEC_USER_MEM_SIZE;
 aSecureAreas[0].startAddress = SFU_SEC_USER_MEM_START_FROM_OB;
 aSecureAreas[0].removeDuringBankErase = 1U;
 /* Only 1 secure area is used */
 aSecureAreas[1].sizeInBytes = 0U;
 aSecureAreas[1].startAddress = 0U;
 aSecureAreas[1].removeDuringBankErase = 1U;

 TRACE("\r\n= [SBOOT] SecArea.size: %d SecArea.addr:%x - RESET", aSecureAreas[0].sizeInBytes,
 aSecureAreas[0].startAddress);

 /* no need to set pbIsProtectionToBeApplied and e_ret_status because the next function triggers a RESET */
 SFU_LL_RSS->resetAndInitializeSecureAreas(1, aSecureAreas);

#else
 TRACE("\r\n= [SBOOT] System Security Configuration failed: Secure User Memory is incorrect. STOP!");
 SFU_EXCPT_Security_Error();
#endif /* SECBOOT_OB_DEV_MODE */
 }

 return e_ret_status;
}

 


@Jocelyn RICARD, @Fred 

This topic has been closed for replies.
Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
May 28, 2024

Hello @aco990 ,

The STM32H743 does not support the secure memory, only STM32H753.

Example provided in SBSFU is for NUCLEO-H753ZI

Difference between the 2 chips is only related to security : Secure memory and crypto accelerator.

Best regards

Jocelyn

 

3 replies

aco990Author
Associate III
May 27, 2024

And after calling HAL_FLASH_OB_Launch(); the SECURITY Bit in OPTSR_PRG is not set

aco990_0-1716818116825.png

 

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
May 28, 2024

Hello @aco990 ,

The STM32H743 does not support the secure memory, only STM32H753.

Example provided in SBSFU is for NUCLEO-H753ZI

Difference between the 2 chips is only related to security : Secure memory and crypto accelerator.

Best regards

Jocelyn

 

aco990Author
Associate III
May 28, 2024

Yes, thank you @Jocelyn RICARD  for replying! I also saw it yesterday in the datasheet that it doesn't support it