Skip to main content
PBrai.1
Visitor II
Dec 14, 2022 5:37 PM UTC
Question

On the STM32H (not L) I need to use a 1-wire EPROM, and I try the generic driver calls generated by the IDE (HAL_SWPMI_Receive, HAL_SWPMI_Transmit, HAL_SWPMI_MspInit, etc.) and I see no bits going out on the scope, and the transmit times out.

I can "Transmit" but the TXE flag never clears and the transmit times out. It's unclear which parts of the bus are fully automated (reset, discovery, etc.) and how much of the CRC is handled, etc. I can see nothing on a scope, but if the chip gets in an odd state and never tries to send that would match what I'm seeing. Without better register descriptions or some example that can talk to a 1wire EPROM I'm kinda stuck.

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Dec 14, 2022 6:12 PM UTC

All the peripheral and pin clocks are enabled?

Are all the peripheral registers reporting zero?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Dec 14, 2022 6:16 PM UTC

The STM32H7xx of some description? It helps to be very specific as there are literally thousands of STM32 parts, and at least half a dozen different H7 die in circulation.

Show the salient peripheral, pin, clock initialization code, and usage.

https://st-onlinetraining.s3.amazonaws.com/STM32H7-Peripheral-Single-Wire-Protocol-Master-Interface_%28SWPMI%29/index.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..