Skip to main content
Steve Melnikoff
Senior
February 6, 2026
Question

OEMiROT: bug in external flash config (stm32_extmem_conf.h)

In STM32Cube_FW_H7RS_V1.3.0, file Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Boot\Inc\stm32_extmem_conf.h:

The configuration for the external RAM (presumably for an APS256XXN-OBR-BG, since that's what on the DK) is incorrect. In particular, it doesn't set the latency values to be able to run at 200 MHz.

(I think that the dummy cycle values may also be wrong - but I suspect they're ignored anyway.)

Here's my code (I also changed the drive strength, but that may not be necessary). Without these changes, the RAM could be read, but not written:

 .PsramObject =
 {
 .psram_public = {
 .MemorySize = HAL_XSPI_SIZE_256MB, /* memory size is 256Mbit */
 .FreqMax = 200000000u, /* 200Mhz */
 .NumberOfConfig = 3,
 /* Config */
 {
#define EXTRAM_MR0_READ_LATENCY_MASK (0x7 << 2)
#define EXTRAM_MR0_DRIVE_STRENGTH_HALF (0x1 << 0)
#define EXTRAM_MR0_READ_LATENCY_200_MHz (0x4 << 2)
#define EXTRAM_MR0_DRIVE_STRENGTH_MASK (0x3 << 0)
#define EXTRAM_MR4_WRITE_LATENCY_MASK (0x7 << 5)
#define EXTRAM_MR4_WRITE_LATENCY_200_MHz (0x1 << 5)
#define EXTRAM_MR8_MODE_MASK (1 << 6)
#define EXTRAM_MR8_MODE_X16 (1 << 6)
 {.WriteMask = EXTRAM_MR8_MODE_MASK, .WriteValue = EXTRAM_MR8_MODE_X16, .REGAddress = 0x08},
 {.WriteMask = EXTRAM_MR0_READ_LATENCY_MASK | EXTRAM_MR0_DRIVE_STRENGTH_MASK,
 .WriteValue = EXTRAM_MR0_READ_LATENCY_200_MHz | EXTRAM_MR0_DRIVE_STRENGTH_HALF, .REGAddress = 0x00},
 {.WriteMask = EXTRAM_MR4_WRITE_LATENCY_MASK, .WriteValue = EXTRAM_MR4_WRITE_LATENCY_200_MHz, .REGAddress = 0x04},
 },

 /* Memory command configuration */
 .ReadREG = 0x40u,
 .WriteREG = 0xC0u,
 .ReadREGSize = 2,
 .REG_DummyCycle = 6u,

 .Write_command = 0xA0u,
 .Write_DummyCycle = 6u,
 .Read_command = 0x20u,
 .WrapRead_command = 0x00u,
 .Read_DummyCycle = 6u,
 }

and as a diff:

SteveMelnikoff_0-1770400544680.png

 

 

1 reply

Amel NASRI
ST Technical Moderator
April 2, 2026

Hi @Steve Melnikoff ,

Your feedback is shared with development team and should be considered in future deliveries.

Internal ticket number: CDM0059390.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.