Skip to main content
Associate
Apr 23, 2025 7:57 PM UTC
Solved

OBKey config file

Hi everyone,

We're working with STiROT and TrustZone on an STM32H5 (NUCLEO-H533RE), and during the provisioning process we generate the STiRoT_Config.obk file from the STiRoT_Config.xml using the Trusted Package Creator (TPC).

Our question is whether the .obk file itself is encrypted or signed during generation, and if so, which keys are used for that purpose?
We're trying to determine if we need to protect any additional private keys used during .obk creation, beyond those already defined for firmware encryption and authentication.

Any insight on whether the .obk file is cryptographically protected (encrypted or signed), or if it's simply a binary container holding the public and private keys for secure boot, would be greatly appreciated.

Thanks in advance!


This topic has been closed for replies.
Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Apr 23, 2025 8:36 PM UTC

Hello @lautiq ,

You can find the details of the obk format in AN6007 here

This is in Appendix C

The content is not encrypted. Only protected with a hash for integrity check

Best regards

Jocelyn

2 replies

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Apr 23, 2025 8:36 PM UTC

Hello @lautiq ,

You can find the details of the obk format in AN6007 here

This is in Appendix C

The content is not encrypted. Only protected with a hash for integrity check

Best regards

Jocelyn

lautiqAuthor
Associate
Apr 24, 2025 12:37 PM UTC

Thank you very much @jocelyn,
That answers my question clearly. I appreciate your help!