Skip to main content
vsing.1
Associate II
Apr 27, 2022 11:47 AM UTC
Question

Not able to jump to application after enabling HDP

@JHOUD​ @TDK​ @Dimitrios Bako​ 

I have configured HDP as follows :

0693W00000LzCUYQA3.pngBy Bootloader .icf details are :

define symbol __ICFEDIT_region_ROM_start__       = 0x0C000800;

define symbol __ICFEDIT_region_ROM_end__        = 0x0C007FFF;

Configurations when i debug the code are also fine :

0693W00000LzCVgQAN.pngNow from Bootloader i Jump to my secure application in which i Enable Hide protection :

HAL_FLASHEx_EnableSecHideProtection(FLASH_BANK_1);

issue is after this i am not able to jump to my nonsecure application. .icf details are:

define symbol __ICFEDIT_intvec_start__ = 0x08020000;

/*-Memory Regions-*/

define symbol __ICFEDIT_region_ROM_start__   = 0x08020800;

define symbol __ICFEDIT_region_ROM_end__    = 0x08027FFF;

without enabling Hide protection it works fine.

Am i missing something?

This topic has been closed for replies.

4 replies

TDK
Apr 27, 2022 2:17 PM UTC
Not my area of expertise, sorry.
"If you feel a post has answered your question, please click ""Accept as Solution""."
vsing.1
vsing.1Author
Associate II
Apr 27, 2022 2:42 PM UTC

if possible ...can you direct it to someone ?

Bubbles
ST Employee
May 3, 2022 8:39 AM UTC

Hi, I assume it's a U5, but can you be more specific about the product next time?

When you say not able to jump, what exactly happens? security exception, hard fault?

I haven't yet encountered a problem like this, HDP only does what the RM says, makes a portion of Flash inaccessible until reset.

Are you sure there is no access to that HDP area?

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
vsing.1
vsing.1Author
Associate II
May 3, 2022 3:37 PM UTC

Hi @JHOUD​ 

yes device is STM32U575.

Code is divided into 3 Applictions :

  1. Bootloader
  2. Secure App
  3. Non Secure App

HDP is applied on Bootloader region:

i.e WMHDPEndPage = 3 of Bank 1

Code jumps to secure App from Bootloader App :

Hide Protection access disabled in Secure App.

HAL_FLASHEx_EnableSecHideProtection(FLASH_BANK_1);

Secure App then jumps to Non-secure App :

here firmware kind of hangs and program counter shows

[PC = 0xefff'fffe]

I have checked HDP by applying it to BANK 2 ,which is working fine.

But when i am applying it to Bank1 (where my code lies) this issue occurs.

I am detailing memory segregation below ,because it seems like jumping to non-secure app is accessing HDP region somehow.

BOOTLOADER APP:

/*-Specials-*/

define symbol __ICFEDIT_intvec_start__ = 0x0C000000;

/*-Memory Regions-*/

define symbol __ICFEDIT_region_ROM_start__       = 0x0C000800;

define symbol __ICFEDIT_region_ROM_end__        = 0x0C007FFF;

define symbol __ICFEDIT_region_ROM_static_data_start__ = 0x0C008000;

define symbol __ICFEDIT_region_ROM_static_data_end__  = 0x0C00BFFF;

define symbol __ICFEDIT_region_ROM_dynamic_data_start__ = 0x0C00C000;

define symbol __ICFEDIT_region_ROM_dynamic_data_end__  = 0x0C00FFFF;

define symbol __ICFEDIT_region_RAM_start__       = 0x30000000;

define symbol __ICFEDIT_region_RAM_end__        = 0x3002FFFF;

SECURE APP:

/*-Specials-*/

define symbol __ICFEDIT_intvec_start__ = 0x0C010000; // add memory for keys

/*-Memory Regions-*/

define symbol __ICFEDIT_region_ROM_start__   = 0x0C010800;

define symbol __ICFEDIT_region_ROM_end__    = 0x0C017FFF;

define symbol __ICFEDIT_region_ROM_NSC_start__ = 0x0C018000;

define symbol __ICFEDIT_region_ROM_NSC_end__  = 0x0C01FFFF;

define symbol __ICFEDIT_region_RAM0_start__   = 0x30000000;

define symbol __ICFEDIT_region_RAM0_end__    = 0x3002FFFF;

define symbol __ICFEDIT_region_RAM1_start__   = 0x30030000;

define symbol __ICFEDIT_region_RAM1_end__    = 0x30037FFF;

define symbol __ICFEDIT_region_RAM2_start__   = 0x30038000;

define symbol __ICFEDIT_region_RAM2_end__    = 0x3003FFFF;

NON-SECURE APP:

/*-Specials-*/

define symbol __ICFEDIT_intvec_start__ = 0x08020000;

/*-Memory Regions-*/

define symbol __ICFEDIT_region_ROM_start__   = 0x08020800;

define symbol __ICFEDIT_region_ROM_end__    = 0x08027FFF;

define symbol __ICFEDIT_region_RAM_start__   = 0x20040000;

define symbol __ICFEDIT_region_RAM_end__    = 0x20057FFF;

Adding few details when issue occur:

0693W00000Np75CQAR.png0693W00000Np75WQAR.png