Skip to main content
crwper
Senior
Mar 11, 2021 4:54 PM UTC
Solved

"Multiple definition" when compiling SBSFU v2.4.0 for STM32WB55

I've been able to compile previous versions of SBSFU (P-NUCLEO-WB55.Nucleo/Applications/1_Image) without issues, but with this one I've run into two issues:

First, SE code did not fit in SE_ROM_region. I was able to fix this by adjusting the linker map and MPU region definitions.

Second, I get this error when compiling the UserApp project:

c:\st\stm32cubeide_1.1.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../../1_Image_SBSFU/SW4STM32/STM32WB55RG_Nucleo_1_Image_SBSFU/Debug\se_interface_app.o: in function `SE_APP_GetActiveFwInfo':
(.SE_IF_Code+0x0): multiple definition of `SE_APP_GetActiveFwInfo'; ../../../../1_Image_SBSFU/SW4STM32/STM32WB55RG_Nucleo_1_Image_SBSFU/Debug\se_interface_app.o:(.SE_IF_Code+0x0): first defined here

If I search the SBSFU projects for "SE_APP_GetActiveFwInfo", I find the definition in se_interface_application.c (in the SBSFU project), the declaration in se_interface_application.c (also in the SBSFU project) and a single call in se_user_code.c (in the UserApp project). It's hard for me to see how there could be multiple definitions here. Any debugging advice would be greatly appreciated.

Thanks!

This topic has been closed for replies.
Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Mar 11, 2021 5:40 PM UTC

Hello,

this build issue is very probably the same described here:

https://community.st.com/s/question/0D53W00000cRsLASA0/the-update-to-cubeide-160-cause-a-linker-error-compiling-the-userapp

This is related to latest release 1.6.0 of STM32CubeIDE. The solution is provide in this other post.

Best regards

Jocelyn

3 replies

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Mar 11, 2021 5:40 PM UTC

Hello,

this build issue is very probably the same described here:

https://community.st.com/s/question/0D53W00000cRsLASA0/the-update-to-cubeide-160-cause-a-linker-error-compiling-the-userapp

This is related to latest release 1.6.0 of STM32CubeIDE. The solution is provide in this other post.

Best regards

Jocelyn

crwper
crwperAuthor
Senior
Mar 11, 2021 6:29 PM UTC

That did it. Thanks again!

Amin.TAYEBI
Associate II
Jul 7, 2021 1:24 PM UTC

Hi

I solved the problem by disconnecting and connecting the stm32-wl55c1 from my PC while pressing Debug botton in Cube-IDE.

Amin TAYEBI