Skip to main content
SPati.7
Associate III
June 27, 2022
Solved

is ACTIVE SLOT Header protected ??

From SBSFU examples, with default SECUSER memory setting except reading from OB registers, it is only protecting SBSFU area alone.

Are we need to protect SBSFU + ACT_SLOT HEADER (1024 Bytes for H7) area as well right ??

So what is your recommendation on protection of HEADER ??

This topic has been closed for replies.
Fred
FredBest answer
ST Employee
June 28, 2022

Ok, there is indeed a bug.

A change made for H7 devices with non-contiguous headers has been propagated erroneously to all H7 devices.

Will be better with:

#define SFU_SEC_MEM_AREA_ADDR_END ((uint32_t) (SlotHeaderAdd[SLOT_ACTIVE_1] + SFU_IMG_IMAGE_OFFSET - 1U))

in:

Firmware/Projects/NUCLEO-H753ZI/Applications/2_Images/2_Images_SBSFU/SBSFU/Target/sfu_low_level_security.h

Sorry for any inconvenience.

17 replies

Fred
ST Employee
June 27, 2022

It protects also the active slot header:

0693W00000NspYxQAJ.png

Fred
ST Employee
June 27, 2022

When this is called:

SFU_MPU_SysCall((uint32_t)SB_SYSCALL_LAUNCH_APP, SlotStartAdd[SlotNumber] + SFU_IMG_IMAGE_OFFSET);

Can you still access the active slot header ?

SPati.7
SPati.7Author
Associate III
June 28, 2022

@Fred​  To launch the application, we are giving right address by passing SlotStartAdd[SlotNumber] + SFU_IMG_IMAGE_OFFSET. But question is on configuring the secure user memory protection.

From examples, i didn't see that we are applying secure user memory protection to ACT_SLOT Header part.

So, as you mentioned, we should protect ACT SLOT HEADER as well, while configuring through OB, right ??

Fred
ST Employee
June 28, 2022

Yes, the active slot header is a sensitive piece of information, it must be protected otherwise we cannot trust the authenticity and integrity checks.

So, from a design perspective, it is clear that it must be protected.

Now, when looking at the latest implementation, I think the size we protect is too short.

I'm trying to clarify it with my colleagues.

Fred
ST Employee
June 27, 2022

Reading the code, I have a doubt too...let me check further.

Fred
FredBest answer
ST Employee
June 28, 2022

Ok, there is indeed a bug.

A change made for H7 devices with non-contiguous headers has been propagated erroneously to all H7 devices.

Will be better with:

#define SFU_SEC_MEM_AREA_ADDR_END ((uint32_t) (SlotHeaderAdd[SLOT_ACTIVE_1] + SFU_IMG_IMAGE_OFFSET - 1U))

in:

Firmware/Projects/NUCLEO-H753ZI/Applications/2_Images/2_Images_SBSFU/SBSFU/Target/sfu_low_level_security.h

Sorry for any inconvenience.

SPati.7
SPati.7Author
Associate III
June 29, 2022

@Fred​  Thanks for your prompt replies.

I want to give appreciation for your help, we are getting, May i know the channel to do the same.

Fred
ST Employee
August 1, 2022

Hi,

sorry for the late reply, I was on holidays.

The crypto scheme is like this:

0693W00000QMal1QAD.png

SPati.7
SPati.7Author
Associate III
August 1, 2022

@Fred​  Thank you very much for reply.

By default is this is the signing mechanism we follow or Do we configure to SIGN alone metadata header with SHA256 of Metadata Header.??

Looks to me, we compute SHA256 of Firmware, add this TAG in metadata header and sign Metadata header from example. is this correct ??

Rejane Durand
Visitor II
September 1, 2022

Hello,

This is correct. This is the signing mechanism followed by the software.

Both tags are checked during the update:

0693W00000SuJmrQAF.jpg