Skip to main content
martinhaefner9
Associate III
Jun 4, 2025 1:39 PM UTC
Question

internal temperatur sensor calibration value with TZEN

Hello together,

 

i have an application running with TZEN, unfortunately the readings of the internal temperature sensor calibration values are always zero.

Is there a secure address where the values are stored ?

Or any chance to get the values out in TZEN mode ?

As @Jocelyn RICARD knows i had to enable the trust zone to do the embeddeed provisioning

 

Kind regards

Martin 

This topic has been closed for replies.

1 reply

Jocelyn RICARD
ST Employee
Jun 13, 2025 5:48 PM UTC

Hello @martinhaefner9 ,

this issue should not be related to TrustZone.

The access to system memory where calibration values is located is constrained.

You need to either disable ICache or add a MPU region to disable the cache only on this area.

You can find this in example: 

STM32Cube_FW_H5_V1.5.0\Projects\NUCLEO-H563ZI\Examples_LL\UTILS\UTILS_ReadDeviceInfo\

I made the test on non secure side of a TrustZone project

Here is the simple MPU configuration I added:

void MPU_Config(void)
{
 MPU_Region_InitTypeDef MPU_InitStruct = {0};
 MPU_Attributes_InitTypeDef MPU_AttributesInit = {0};

 /* Disables the MPU */
 HAL_MPU_Disable();

 /** Initializes and configures the Region 0 and the memory to be protected
 */
 MPU_InitStruct.Enable = MPU_REGION_ENABLE;
 MPU_InitStruct.Number = MPU_REGION_NUMBER0;
 MPU_InitStruct.BaseAddress = 0x08FFF000;
 MPU_InitStruct.LimitAddress = 0x08FFFFFFU;
 MPU_InitStruct.AttributesIndex = MPU_ATTRIBUTES_NUMBER0;
 MPU_InitStruct.AccessPermission = MPU_REGION_ALL_RO;
 MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
 MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;

 HAL_MPU_ConfigRegion(&MPU_InitStruct);

 /** Initializes and configures the Attribute 0 and the memory to be protected
 */
 MPU_AttributesInit.Number = MPU_ATTRIBUTES_NUMBER0;
 MPU_AttributesInit.Attributes = INNER_OUTER(MPU_NOT_CACHEABLE);

 HAL_MPU_ConfigMemoryAttributes(&MPU_AttributesInit);
 /* Enables the MPU */
 HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

}

 

Best regards

Jocelyn