Skip to main content
Pmare.11
Associate
Mar 22, 2021 4:36 PM UTC
Solved

Impossible to load UserApp (sfb file) using TeraTerm or Minicom. The terminal is always stuck at the first block transfer.

Hello, I a new with NUCLEO STM32H753ZI and trying the SBSFU examples (1 and 2 images). I can flash and launch the SBSFU but I can't load any user application (userapp.sfb)

I use STM32 tools, either using Linux or Windows with the same result :

  • I connect with a VCP using Teraterm (on Windows) or Minicom on Linux) with YMODEM protocol,
  • The terminal display the SBSFU sequence, which is good and terminates by waiting for a user appli to be downloaded
  • I Send the UserApp.sfb with (File->Transfer->Ymodem)
  • AND the load remains stopped at the first block ....

I have followed the guides given in the examples documentation (from readme files into project SBSFU V2.4.0), I have applied :

  • The security configuration (Option Bytes set to Default "No Security")
  • Serial configuration seems also OK
This topic has been closed for replies.
Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Mar 26, 2021 5:40 PM UTC

Hello,

There is a MINICOM flag in the SBSFU code as well as in the user application code in the 2 images setup.

If you don't activate if (which is the default setting) and run on windows, there should be no issue.

On Linux I could see it failing even with MINICOM flag set on some distribution.

So, I recommend fist testing on Windows if possible.

I could check with TeraTerm and extraputty without issue.

So, could you please check again starting with a clean project (from zip file) ?

Best regards

Jocelyn

2 replies

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Mar 26, 2021 5:40 PM UTC

Hello,

There is a MINICOM flag in the SBSFU code as well as in the user application code in the 2 images setup.

If you don't activate if (which is the default setting) and run on windows, there should be no issue.

On Linux I could see it failing even with MINICOM flag set on some distribution.

So, I recommend fist testing on Windows if possible.

I could check with TeraTerm and extraputty without issue.

So, could you please check again starting with a clean project (from zip file) ?

Best regards

Jocelyn

Pmare.11
Pmare.11Author
Associate
Mar 31, 2021 2:46 PM UTC

Thank you for your reply Richard. I followed your advice and now is works fine. I think I had a problem in the option bytes settings that prevented the correct loading finally.

Best regards

Pascal