Skip to main content
Grogu
Associate III
Jan 6, 2023 12:37 AM UTC
Solved

Implement Key replacement package for Image signing Key ECCKEY1

The SBSFU framework allows users to employ multiple image signing keys, ECCKEY1, ECCKEY2, and ECCKEY3.

Is there a method to blacklist ECCKEY1 and replace it with ECCKEY4, which may be transmitted via a key replacement update package if the private key for ECCKEY1 is leaked/compromised?

Keys are compiled into code and stored in the SE Key region ROM, which is secured by MPU-RX + WRP + PCROP.

Please advise what options I have to replace the key which is compromised?

Assuming bootloader enhanced to differentiate between .sfb and key replacement package.

This topic has been closed for replies.
Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Jan 6, 2023 5:25 PM UTC

Hello @Community member​ 

There is no mechanism to implement such behaviour.

Robustness of SBSFU is relying on the immutability of the code and public key.

So, I have no solution to propose here.

Best regards

Jocelyn

2 replies

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Jan 6, 2023 5:25 PM UTC

Hello @Community member​ 

There is no mechanism to implement such behaviour.

Robustness of SBSFU is relying on the immutability of the code and public key.

So, I have no solution to propose here.

Best regards

Jocelyn

Grogu
GroguAuthor
Associate III
Jan 9, 2023 3:44 AM UTC

Thanks @Jocelyn RICARD​