Skip to main content
SteveC
Associate
Jun 26, 2020 9:02 AM UTC
Question

I'm running Win10 in Fusion on a Mac. It detects the 552 but not the 476

..

    This topic has been closed for replies.

    2 replies

    Jocelyn RICARD
    ST Employee
    Jun 26, 2020 12:04 PM UTC

    Hello Steve,

    this is a setup we cannot reproduce.

    Could you open the device manager ?

    Normally, when plugging a board, you should see the update.

    Also, when plugging the STM32L476 you should see the LED1 and LED3 active.

    Best regards

    Jocelyn

    SteveC
    SteveCAuthor
    Associate
    Jun 26, 2020 1:39 PM UTC

    SOLVED! When it first failed I change the USB lead. It didn't work with the second lead either. I should have tried a third lead! Now with a third lead everything is fine. Worth nothing that not all USB leads are the same! Thanks STM for your support :)