Skip to main content
AFaya.1
Associate III
May 27, 2022 7:29 AM UTC
Question

I am working on stm32h753zi sbsfu part. I am facing the swap issue, and attached the log below.

======================================================================

=       (C) COPYRIGHT 2017 STMicroelectronics         =

=                                  =

=       Secure Boot and Secure Firmware Update        =

======================================================================

= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL

= [SBOOT] STATE: CHECK STATUS ON RESET

 INFO: A Reboot has been triggered by a Software reset!

 INFO: Last execution status before Reboot was:Executing Fw Image.

 INFO: Last execution detected error was: No error. Success.

= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD

= [SBOOT] STATE: CHECK USER FW STATUS

 New Fw to be installed from slot SLOT_DWL_1

= [SBOOT] STATE: INSTALL NEW USER FIRMWARE 

= [SBOOT] RuntimeProtections: 0

 612480 bytes of ciphertext decrypted.

 Image preparation done.

 Swapping the firmware images

= [FWIMG] Swap process failure!

=     Installation procedure cannot be finalized!

= [FWIMG] FW installation failed!

= [SBOOT] STATE: HANDLE CRITICAL FAILURE

= [EXCPT] NOT POSSIBLE TO SWAP IMAGES!

= [SBOOT] STATE: REBOOT STATE MACHINE

========= End of Execution ==========

In function : SwapFirmwareImages(ActiveSlot, DwlSlot, pTestHeader)

Both read and write slots are same these condition code was failed.

if (index_dwl_slot_read >= index_dwl_slot_write)

{

  return SFU_ERROR;

} 

Please give me the guidance for fix this issue.

Thanks,

This topic has been closed for replies.

1 reply

Bubbles
ST Employee
May 27, 2022 1:21 PM UTC

Hi @AFaya.1​ ,

the code comment should explain this - the download slot is not large enough to handle this as partial image. Maybe you did not intend to handle the upload as partial image - then the whole slot (7x128k by default) can be used.

See the partial image chapter in the user manual for more info.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.