Skip to main content
saico
Associate
Feb 17, 2020 3:41 AM UTC
Question

I am learning about X-CUBE-AWS examples, when update from OTA, I get a SIGNATURE CHECK FAILED exception, somebody can help me to resolve this problem?

I download X-CUBE-AWS 1.4.0 to compile and install on my STM32F769IDISCOVERY board, everything running ok, but when I configure it to update new app version from OTA, after reboot is shows:

= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL

= [SBOOT] STATE: CHECK STATUS ON RESET

     INFO: A Reboot has been triggered by a Software reset!

     Consecutive Boot on error counter reset 

     Consecutive Boot on error counter = 0 

     Consecutive Boot on error counter updated 

     INFO: Last execution status before Reboot was:Executing Fw Image.

     INFO: Last execution detected error was:No error. Success.

= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD

= [SBOOT] STATE: CHECK USER FW STATUS

     New Fw Encrypted, to be decrypted

= [SBOOT] STATE: INSTALL NEW USER FIRMWARE 

     262080 bytes of ciphertext decrypted.

= [FWIMG] The decrypted image is incorrect!

= [FWIMG] FW installation failed!

= [SBOOT] STATE: HANDLE CRITICAL FAILURE

= [EXCPT] SIGNATURE CHECK FAILED!

= [SBOOT] STATE: REBOOT STATE MACHINE

========= End of Execution ==========

where is the problem?

This topic has been closed for replies.

2 replies

asala.19
Associate III
Apr 27, 2020 6:21 AM UTC

Hi,

I am facing same type of issue. have you resolve the above issue?

Thanks,

Arjun

NKuma.9
Associate
Jul 14, 2021 12:24 PM UTC

hello

iam also facing the same issue. Any solutions?

thank you

nithish