Skip to main content
DBark.2
Associate II
May 28, 2021 12:11 AM UTC
Question

How to use the STM32 Hardware CRC to calculate Ethernet/GFP CRC

I've managed to configure the STM32 CRC such that it can create the standard CRC-32 as per this article - https://stackoverflow.com/questions/39646441/how-to-set-stm32-to-generate-standard-crc32. However, this CRC does not match Ethernet spec.

Is there a way to configure the STM32 Hardware CRC peripheral such that it can create valid Ethernet/GFP crc values?

I already have software that can generate the CRC. I'm specifically looking to see if there is a way to utilize the faster speeds of the CRC hardware generation.

This topic has been closed for replies.

3 replies

TDK
May 28, 2021 12:18 AM UTC

Which STM32? Some are configurable, some are not. Non-configurable uses 0x04C11DB7 as the polynomial, at least for STM32F4, which is ethernet. You'd have to explain your input, what you're getting, and what you're expecting. There are some details since STM32 processes bytes assuming little-endian format.

"If you feel a post has answered your question, please click ""Accept as Solution""."
DBark.2
DBark.2Author
Associate II
May 28, 2021 12:39 AM UTC

Both CRC-32 in question are using a polynomial of 0x04C11DB7. I'm using byte input data inversion mode to handle the endian problem.

My current configuration is on an STM32L5

 hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;
 hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;
 hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_BYTE;
 hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_ENABLE;
 hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
 if (HAL_CRC_Init(&hcrc) != HAL_OK)

I'm inverting the data after receiving it to get values that match other expected CRC.

My input is a binary file, my output matches different non-ethernet CRC32

I want my output to match ethernet CRC-32.

TDK
May 28, 2021 12:48 AM UTC
If you give a complete example with data, received values, and expected values, I will track it down for you, but I’m not going to guess at what you want. Preferably an example with 4 bytes of input data.
"If you feel a post has answered your question, please click ""Accept as Solution""."