Skip to main content
Visitor II
May 8, 2026
Question

how to use RTX5 with Root of Trust on NUCLEO-N657X0-Q ?

I am a user of the NUCLEO-N657X0-Q board.
I would like to use Keil MDK RTX5 RTOS together with Root of Trust.
My development environment is as follows:
1> Development tool: Keil uVision V5.42
2> Example source: STM32Cube\Repository\STM32Cube_FW_N6_V1.2.0\Projects\NUCLEO-N657X0-Q\Applications\ROT\OEMuROT_Appli
3> Development board: NUCLEO-N657X0-Q

4> Manage Run-Time Environment Setting

young_seo_0-1778228471715.png

 

I have added the osKernelInitialize() function to the main function as shown below.

int main(void)
{
#ifdef PRINT_BOOT_TIME
 /* Get boot cycles */
 end = DWT->CYCCNT;
#endif

 /* Reset of all peripherals, Initializes the Flash interface and the systick. */
 HAL_Init();

#ifdef PRINT_BOOT_TIME
 /* Get Boot Time */
 time = ((uint64_t)(end) * 1000U / SystemCoreClock);
#endif

 /* Register SecureFault callback defined in non-secure and to be called by secure handler */
 SECURE_RegisterCallback(SECURE_FAULT_CB_ID, (void *)SecureFault_Callback);

 /* Register SecureError callback defined in non-secure and to be called by secure handler */
 SECURE_RegisterCallback(IAC_ERROR_CB_ID, (void *)SecureError_Callback);
 osKernelInitialize() ; // Add

 /*******************************************************************************
 * Common Configuration Routines *
 *******************************************************************************/
 pUserAppId = (uint8_t *)&UserAppId;
 COM_Init();

 printf("\r\n======================================================================");
 printf("\r\n= TEST TEST");
 printf("\r\n======================================================================");
 printf("\r\n\r\n");
}

When executed, the serial messages appear for a while and then stop, and the SecureFault_Callback() function is called, after which the program does not proceed any further.

 

I am inquiring about the issue of the program stopping. Thank you.


Edited to apply source code formatting - please see How to insert source code for future reference.

1 reply

Andrew Neil
Super User
May 8, 2026

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

 


@young_seo wrote:

 Keil MDK RTX5 RTOS together with Root of Trust


That's a Keil product - not ST - so have you asked Keil about this?

https://developer.arm.com/Tools%20and%20Software/Keil%20MDK/RTX5%20RTOS

https://community.arm.com/support-forums/f/keil-forum 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.