Skip to main content
Visitor II
June 16, 2026
Question

How to use RTC while using Root of Trust on the NUCLEO-N657X0-Q board.

I am a user of the NUCLEO-N657X0-Q board.

 

I am using the NUCLEO-N657X0-Q board with Root of Trust enabled, and I want to use the RTC.
Out of the 3 stages  (FSBL → Secure App → Non-Secure App)  I want to use the RTC in the Non-Secure App.

 

My development environment is as follows:
1> Development tool: Keil uVision V5.42
2> Example source: STM32Cube\Repository\STM32Cube_FW_N6_V1.2.0\Projects\NUCLEO-N657X0-Q\Applications\ROT\OEMuROT_Appli
3> Development board: NUCLEO-N657X0-Q

 

The biggest problem is that when HAL_RTC_Init() is called in the Non-Secure App, it hangs.

 

The source for STM32Cube_FW_N6_V1.2.0\Projects\NUCLEO-N657X0-Q\Applications\ROT\OEMuROT_Appli was created by referencing STM32Cube_FW_N6_V1.2.0\Projects\STM32N6570-DK\Applications\ROT\OEMuROT_Appli.

 

The code I added is as follows.

1. Added to the main function of the Secure App.

HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RCC_PERIPH_INDEX_RTC, RIF_ATTRIBUTE_NSEC);




2. Added a function to the Non-Secure App.


RTC_HandleTypeDef RtcHandle;

void rtc_Init(void)
{
memset(&RtcHandle, 0, sizeof(RTC_HandleTypeDef));

RtcHandle.Instance = RTC;
RtcHandle.Init.HourFormat = RTC_HOURFORMAT_24;
RtcHandle.Init.AsynchPrediv = 0x7F;
RtcHandle.Init.SynchPrediv = 0xF9;
RtcHandle.Init.OutPut = RTC_OUTPUT_DISABLE;
RtcHandle.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
RtcHandle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
RtcHandle.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
RtcHandle.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
RtcHandle.Init.BinMode = RTC_BINARY_NONE;

printf("rtc_Init() start 111...\r\n");

if (HAL_RTC_Init(&RtcHandle) != HAL_OK)
{
printf("rtc_Init() Fail!\r\n");
return;
}
printf("rtc_Init() OK!\r\n");
}



void HAL_RTC_MspInit(RTC_HandleTypeDef *hrtc)
{
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

if (hrtc->Instance == RTC)
{
HAL_PWR_EnableBkUpAccess();

PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) ;


__HAL_RCC_RTC_CLK_ENABLE();
__HAL_RCC_RTCAPB_CLK_ENABLE();

printf("HAL_RTC_MspInit() end...\r\n") ;

}
}


int main(void)
{
.
.
.

#ifdef PRINT_BOOT_TIME
printf("\r\nBoot time : %u ms at %u MHz", (unsigned int)(time), (unsigned int)(SystemCoreClock/1000000U));
printf("\r\n");
#endif
printf("\r\n======================================================================");
printf("\r\n= (C) COPYRIGHT 2024 STMicroelectronics =");
printf("\r\n= =");
printf("\r\n= User App #%c =", *pUserAppId);
printf("\r\n======================================================================");
printf("\r\n\r\n");

/* User App firmware runs*/

rtc_Init() ;

FW_APP_Run();

.
.
.


}


 

 

The execution result is as follows.

 

======================================================================
              (C) COPYRIGHT 2024 STMicroelectronics                 =
                                                                    =
                          User App #A                               =
======================================================================

rtc_Init() start 111...
HAL_RTC_MspInit() end…

 

 

 

 

 

if (HAL_RTC_Init(&RtcHandle) != HAL_OK) //// ==> It hangs at this point.

 

 

I would like to inquire about how to use RTC in a ROT (Root of Trust) environment.
The actual RTC usage is in the Non-Secure App.

 

Thank you.