Skip to main content
taunboel
Associate
July 4, 2022
Solved

How to use OTFDEC with stm32u5 and Zephyr

Hey, I'm starting on using OTFDEC for encryption of data on external OSPI flash, the project i'm working on is based on the Zephyr OS, and as far as i can see there are no examples on how to build an application with the OTFDEC setup using Zephyr. So is it possible to use OTFDEC with zephyr, and how?

This topic has been closed for replies.
Mohamed Aymen HZAMI
ST Employee
July 27, 2022

Hello @Tobias Aunbøl​ and welcome to the community,

It possible to use OTFDEC with zephyr or any kind of RTOS, or even an application that does not use any RTOS.

The idea is to directly call OTFDEC HAL API in the application. For more information on how to allow use of Cube HAL in application, see this LINK.

There is also an example under the TM32Cube_FW_U5, below the path to the project:

"STM32Cube_FW_U5_V1.1.0\Projects\B-U585I-IOT02A\Examples\OTFDEC\OTFDEC_Data_Decrypt"

Mohamed Aymen

1 reply

Mohamed Aymen HZAMI
ST Employee
July 27, 2022

Hello @Tobias Aunbøl​ and welcome to the community,

It possible to use OTFDEC with zephyr or any kind of RTOS, or even an application that does not use any RTOS.

The idea is to directly call OTFDEC HAL API in the application. For more information on how to allow use of Cube HAL in application, see this LINK.

There is also an example under the TM32Cube_FW_U5, below the path to the project:

"STM32Cube_FW_U5_V1.1.0\Projects\B-U585I-IOT02A\Examples\OTFDEC\OTFDEC_Data_Decrypt"

Mohamed Aymen