Skip to main content
HJung.2
Associate II
Jul 8, 2021 6:41 AM UTC
Question

How to Program stm32f103rc using j-Link when RDP enabled?

Hello.

I'm trying to program the main flash memory of STM32F103RCT6 using J-Link while RDP is enabled.

I followed main flash memory programming procedure in PM0075 manual.

the procedure is in below picture.

0693W00000Bd7ZLQAZ.pngWhen only RDP is enabled, I unlocked Flash_CR_LOCK bit and then Write FLASH_CR_PG to 1.

After this procedure, I tried to write half-word data to 0x080069f0.

However, J-Link reports the error like this.

****** Error: Timeout while calculating CRC, RAMCode did not respond in time. (PC = 0x00000000, CPSR = 0x00000000, LR = 0x01000000)!Failed to erase sectors 14 @ address 0x08006800 ((erase error))

Failed to erase sectors.

Is it impossible to program main flash memory when RDP is enabled?

If not, how can I do it?

Here is my J-Link Commander log.

Device "STM32F103RC (ALLOW OPT. BYTES)" selected.

Connecting to target via JTAG

InitTarget() start

Active read protection detected.

Skipping unsecure.

InitTarget() end

TotalIRLen = 9, IRPrint = 0x0011

JTAG chain detection found 2 devices:

 #0 Id: 0x3BA00477, IRLen: 04, CoreSight JTAG-DP

 #1 Id: 0x06414041, IRLen: 05, STM32 Boundary Scan

DPv0 detected

Scanning AP map to find all available APs

AP[1]: Stopped AP scan as end of AP map has been reached

AP[0]: AHB-AP (IDR: 0x14770011)

Iterating through AP map to find AHB-AP to use

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FF000

CPUID register: 0x411FC231. Implementer code: 0x41 (ARM)

Found Cortex-M3 r1p1, Little endian.

FPUnit: 6 code (BP) slots and 2 literal slots

CoreSight components:

ROMTbl[0] @ E00FF000

ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 001BB000 SCS

ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 001BB002 DWT

ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 000BB003 FPB

ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 001BB001 ITM

ROMTbl[0][4]: E0040000, CID: B105900D, PID: 001BB923 TPIU-Lite

ROMTbl[0][5]: E0041000, CID: B105900D, PID: 101BB924 ETM-M3

Cortex-M3 identified.

J-Link>w4 40022004 45670123

Writing 45670123 -> 40022004

J-Link>w4 40022004 cdef89ab

Writing CDEF89AB -> 40022004

J-Link>mem32 40022010 1

40022010 = 00000000

J-Link>h

PC = 08003FFE, CycleCnt = 3A8FCF29

R0 = E000ED0C, R1 = 05FA0004, R2 = 05FA0004, R3 = 40003000

R4 = 20000924, R5 = 1FFFF810, R6 = 1FFFF810, R7 = 2000BFDC

R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000

R12= 00000000

SP(R13)= 2000BFDC, MSP= 2000BFDC, PSP= 00000000, R14(LR) = FFFFFFF9

XPSR = 01000003: APSR = nzcvq, EPSR = 01000000, IPSR = 003 (HardFault)

CFBP = 00000000, CONTROL = 00, FAULTMASK = 00, BASEPRI = 00, PRIMASK = 00

FPU regs: FPU not enabled / not implemented on connected CPU.

J-Link>w4 40022010 0000001

Writing 00000001 -> 40022010

J-Link>w2 080069f0 1111

Writing 1111 -> 080069F0

J-Link>mem32 4002200c 1

****** Error: Timeout while calculating CRC, RAMCode did not respond in time. (PC = 0x00000000, CPSR = 0x00000000, LR = 0x01000000)!Failed to erase sectors 14 @ address 0x08006800 ((erase error))

Failed to erase sectors.

This topic has been closed for replies.

3 replies

Uwe Bonnes
Chief
Jul 8, 2021 8:35 AM UTC

Reset the option bits to default, meaning no protection. Mass erase of flash happens as result of the RDP downgrade. Then proceed as normal.

HJung.2
HJung.2Author
Associate II
Jul 8, 2021 10:05 AM UTC

Hello, Thank you for your answer.

However, I want to try programming 2 bytes of main flash memory when RDP is enabled not resetting the device.

Thank you

Uwe Bonnes
Chief
Jul 8, 2021 10:21 AM UTC

Carefully read pm0075:

Once the protection byte has been programmed:

   ...

   Pages 0-3 (for low- and medium-density devices), or pages 0-1 (for high-density and

   connectivity line devices) are automatically write-protected. The rest of the memory can

   be programmed by the code executed from the main Flash memory (for IAP, constant

   storage, etc.), but it is protected against write/erase (but not against mass erase) in

   debug mode or when booting from the embedded SRAM.