Skip to main content
RP_it
Associate II
December 28, 2018
Solved

How to include Crypto Library in System workbench project?

0690X000006CvjkQAC.bmpI have Downloaded STM32CubeExpansion_Crypto_V3.1.0 library. I am trying to use it for STM32L431RBTx Microcontroller. But I am getting error as shown in following images.

What am I missing to do?Please help.

Building target:

_V0.1.elf" @"objects.list" -llibSTM32CryptographicV3.0.0_CM4_GCC_ot -lm

c:/ac6/systemworkbench/plugins/fr.ac6.mcu.externaltools.arm-none.win32_1.13.2.201705091103/tools/compiler/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: cannot find -llibSTM32CryptographicV3.0.0_CM4_GCC_ot

collect2.exe: error: ld returned 1 exit status

0690X000006CvcPQAS.bmp0690X000006CvcUQAS.bmp

I have also tried by removing the prefix 'lib' from library .a file name. Then I am getting following error.

Invoking: MCU GCC Linker

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -L"D:\L4\STM32CubeExpansion_Crypto_V3.1.0\Fw_Crypto\STM32L4\Middlewares\ST\STM32_Cryptographic\Lib" -specs=nosys.specs -specs=nano.specs -T"../STM32L431RBTx_FLASH.ld" -Wl,-Map=output.map -Wl,--gc-sections -o "Hotel_Lock_V0.1.elf" @"objects.list" -lSTM32CryptographicV3.0.0_CM4_GCC_ot

c:/ac6/systemworkbench/plugins/fr.ac6.mcu.externaltools.arm-none.win32_1.13.2.201705091103/tools/compiler/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: error: Hotel_Lock_V0.1.elf uses VFP register arguments, D:\L4\STM32CubeExpansion_Crypto_V3.1.0\Fw_Crypto\STM32L4\Middlewares\ST\STM32_Cryptographic\Lib\libSTM32CryptographicV3.0.0_CM4_GCC_ot.a(crypto.o) does not

c:/ac6/systemworkbench/plugins/fr.ac6.mcu.externaltools.arm-none.win32_1.13.2.201705091103/tools/compiler/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file D:\L4\STM32CubeExpansion_Crypto_V3.1.0\Fw_Crypto\STM32L4\Middlewares\ST\STM32_Cryptographic\Lib\libSTM32CryptographicV3.0.0_CM4_GCC_ot.a(crypto.o)

collect2.exe: error: ld returned 1 exit status

make: *** [Hotel_Lock_V0.1.elf] Error 1

This topic has been closed for replies.
Amir NEIFAR
Amir NEIFARBest answer
Visitor II
December 28, 2018

​The new issue is related to the Floating point support.

You need to use another Library built with the support of FPU:

\STM32CubeExpansion_Crypto_V3.1.0\AccHw_Crypto\STM32L4\Middlewares\ST\STM32_Crypto\Lib\libSTM32CryptographicV3.0.0_CM4_GCC_FPU.a

7 replies

Amir NEIFAR
Visitor II
December 28, 2018

Hi,

 This is a link issue, please try to use STM32CryptographicV3.0.0_CM3_GCC without "lib" in the Library name.

Regards,

Amir​

RP_it
RP_itAuthor
Associate II
December 28, 2018

Thanks for your reply Amir. I tried that one also. but getting different error after that.0690X000006CvjuQAC.bmp

0690X000006CvjzQAC.bmp

Amir NEIFAR
Amir NEIFARBest answer
Visitor II
December 28, 2018

​The new issue is related to the Floating point support.

You need to use another Library built with the support of FPU:

\STM32CubeExpansion_Crypto_V3.1.0\AccHw_Crypto\STM32L4\Middlewares\ST\STM32_Crypto\Lib\libSTM32CryptographicV3.0.0_CM4_GCC_FPU.a

RP_it
RP_itAuthor
Associate II
December 28, 2018

Thank you so much Amir for your instant reply. Support of FBU worked. Project built successfully.

Amir NEIFAR
Visitor II
December 28, 2018

​You are welcome.

Good luck for your business.

Happy to support you.

Regards,

Amir NEIFAR

GKush.1
Visitor II
December 11, 2019

thanks Amir

That worked.

Visitor II
October 12, 2023

Getting below error in "...\en.STM32CubeExpansion_Crypto\STM32CubeExpansion_Crypto_V4.1.0\Projects\NUCLEO-L476RG\Applications\Cipher\AES_CBC_EncryptDecrypt\STM32CubeIDE"

rutvas_0-1697112419261.png

Implementing main.c file of AEC_CBC in my existing projects main file, I've included STM32_Cryptographic folder in middlewares