Skip to main content
DLe.4
Associate II
Jan 6, 2023 9:11 AM UTC
Solved

How I can disable Read Out Protection STM32F407 in Level 1?

I tried disable ROP level 1 to level 0 by ST-LINK Utility and STM32CubeProgrammer, but it is not success.

Thanks in advance.

This topic has been closed for replies.
FBLBest answer
ST Technical Moderator
Jan 10, 2023 7:47 AM UTC

Hello @DLe.4​ ,

Please provide more details so that we can help you. You may check the RM0090 for more details. When read protection level 1 is set, there is No access (read, erase, program) to Flash memory or backup SRAM can be performed while the debug feature is connected or while booting from RAM or system memory bootloader. So, a bus error is generated in case of read request.

Could you please share screenshot with STLink utility or CubeProgrammer to understand the issue.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

2 replies

MM..1
Super User
Jan 6, 2023 10:18 AM UTC

Show prog log

FBLBest answer
ST Technical Moderator
Jan 10, 2023 7:47 AM UTC

Hello @DLe.4​ ,

Please provide more details so that we can help you. You may check the RM0090 for more details. When read protection level 1 is set, there is No access (read, erase, program) to Flash memory or backup SRAM can be performed while the debug feature is connected or while booting from RAM or system memory bootloader. So, a bus error is generated in case of read request.

Could you please share screenshot with STLink utility or CubeProgrammer to understand the issue.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL