Skip to main content
STsch.1
Associate III
Dec 28, 2021 8:21 AM UTC
Question

How can I port the SBSFU to another board?

Hi,

I'm using a STM32F446RE Discovery board and would like to test the SBSFU on it. At them moment, I take the example code from the STM32F413H Discovery board, but I'm not sure what I'm doing wrong to never get access over the tera terminal.

What I have done so far according to AN5056 is:

  • Change the flash memory, since the STM32F446RE has only 512kByte

mapping_fwimg.ld:

/*
*****************************************************************************
**
** File : LinkerScript.ld
**
** Abstract : Linker script for STM32F413ZHTx Device with
** 1536KByte FLASH, 320KByte RAM
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used.
**
** Target : STMicroelectronics STM32
**
**
** Distribution: The file is distributed as is, without any warranty
** of any kind.
**
** (c)Copyright Ac6.
** You may use this file as-is or modify it according to the needs of your
** project. Distribution of this file (unmodified or modified) is not
** permitted. Ac6 permit registered System Workbench for MCU users the
** rights to distribute the assembled, compiled & linked contents of this
** file as part of an application binary file, provided that it is built
** using the System Workbench for MCU toolchain.
**
*****************************************************************************
*/
 
/* Slots must be aligned on sector size */
 
/* Active slot #1 (1472 kbytes) */
__ICFEDIT_SLOT_Active_1_start__ = 0x08010000;
__ICFEDIT_SLOT_Active_1_end__ = 0x0807FFFF;
__ICFEDIT_SLOT_Active_1_header__ = __ICFEDIT_SLOT_Active_1_start__;
 
/* Slots not configured */
__ICFEDIT_SLOT_Active_2_header__ = 0x00000000;
__ICFEDIT_SLOT_Active_2_start__ = 0x00000000;
__ICFEDIT_SLOT_Active_2_end__ = 0x00000000;
__ICFEDIT_SLOT_Active_3_header__ = 0x00000000;
__ICFEDIT_SLOT_Active_3_start__ = 0x00000000;
__ICFEDIT_SLOT_Active_3_end__ = 0x00000000;
 

mapping_sbsfu.ld:

/*
*****************************************************************************
**
** File : LinkerScript.ld
**
** Abstract : Linker script for STM32F413ZHTx Device with
** 1536KByte FLASH, 320KByte RAM
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used.
**
** Target : STMicroelectronics STM32
**
**
** Distribution: The file is distributed as is, without any warranty
** of any kind.
**
** (c)Copyright Ac6.
** You may use this file as-is or modify it according to the needs of your
** project. Distribution of this file (unmodified or modified) is not
** permitted. Ac6 permit registered System Workbench for MCU users the
** rights to distribute the assembled, compiled & linked contents of this
** file as part of an application binary file, provided that it is built
** using the System Workbench for MCU toolchain.
**
*****************************************************************************
*/
 
/* SE Code region */
VECTOR_SIZE = 0x200;
__ICFEDIT_SE_Code_region_ROM_start__ = 0x08000000 + VECTOR_SIZE;
__ICFEDIT_SE_CallGate_region_ROM_start__ = __ICFEDIT_SE_Code_region_ROM_start__; /* No need to do +4 as we have dummy bytes in SE_CoreBin .ld file */
__ICFEDIT_SE_CallGate_region_ROM_end__ = __ICFEDIT_SE_Code_region_ROM_start__ + 0x1FF;
 
/* SE key region */
__ICFEDIT_SE_Key_region_ROM_start__ = __ICFEDIT_SE_CallGate_region_ROM_end__ + 0x1;
__ICFEDIT_SE_Key_region_ROM_end__ = __ICFEDIT_SE_Key_region_ROM_start__ + 0xFF;
 
/* SE Startup: call before enabling protection */
__ICFEDIT_SE_Startup_region_ROM_start__ = __ICFEDIT_SE_Key_region_ROM_end__ + 0x1;
__ICFEDIT_SE_Code_nokey_region_ROM_start__ = __ICFEDIT_SE_Startup_region_ROM_start__ + 0x100;
/* Aligned SE End at the end of the 1st 32Kbytes of flash, MPU protection isolation constraints */
__ICFEDIT_SE_Code_region_ROM_end__ = 0x08007FFF;
 
/* SE IF ROM: used to locate Secure Engine interface code */
__ICFEDIT_SE_IF_region_ROM_start__ = __ICFEDIT_SE_Code_region_ROM_end__ + 1;
__ICFEDIT_SE_IF_region_ROM_end__ = __ICFEDIT_SE_IF_region_ROM_start__ + 0x8FF;
 
/* SBSFU Code region */
__ICFEDIT_SB_region_ROM_start__ = __ICFEDIT_SE_IF_region_ROM_end__ + 0x1;
/* Aligned SBSFU end at the end of the 1st 64Kbytes of FLASH, MPU protection isolation constraints */
__ICFEDIT_SB_region_ROM_end__ = 0x0800ffff;
 
SE_Entry_Secure_ROM_Region_Length = __ICFEDIT_SE_CallGate_region_ROM_end__ - __ICFEDIT_SE_CallGate_region_ROM_start__ + 1;
SE_Key_region_ROM_Length = __ICFEDIT_SE_Key_region_ROM_end__ - __ICFEDIT_SE_Key_region_ROM_start__ + 1;
SE_Startup_region_ROM_Length = __ICFEDIT_SE_Code_nokey_region_ROM_start__ - __ICFEDIT_SE_Startup_region_ROM_start__ ;
SE_ROM_region_Length = __ICFEDIT_SE_Code_region_ROM_end__ - __ICFEDIT_SE_Code_nokey_region_ROM_start__ + 1;
SE_IF_region_ROM_Length = __ICFEDIT_SE_IF_region_ROM_end__ - __ICFEDIT_SE_IF_region_ROM_start__ + 1;
SB_ROM_region_Length = __ICFEDIT_SB_region_ROM_end__ - __ICFEDIT_SB_region_ROM_start__ + 1;
 
/* RAM section */
/* SE RAM1 region protected by firewall */
/* SE stack is placed 1st in RAM, stack overflow does not write on other RAM area */
__ICFEDIT_SE_region_RAM_start__ = 0x20000000;
__ICFEDIT_SE_region_RAM_stack_top__ = 0x20000400;
__ICFEDIT_SE_region_RAM_end__ = 0x20000FFF;
 
/* SBSFU RAM1 region */
__ICFEDIT_SB_region_RAM_start__ = __ICFEDIT_SE_region_RAM_end__ + 1;
__ICFEDIT_SB_region_RAM_end__ = 0x2003FFFF;
 
SE_RAM_region_Length = __ICFEDIT_SE_region_RAM_end__ - __ICFEDIT_SE_region_RAM_stack_top__ + 1;
SB_RAM_region_Length = __ICFEDIT_SB_region_RAM_end__ - __ICFEDIT_SB_region_RAM_start__ + 1;
 
MEMORY
{
 SE_Entry_Secure_ROM_Region (rx) : ORIGIN = __ICFEDIT_SE_CallGate_region_ROM_start__, LENGTH = SE_Entry_Secure_ROM_Region_Length
 SE_Key_region_ROM (rx) : ORIGIN = __ICFEDIT_SE_Key_region_ROM_start__, LENGTH = SE_Key_region_ROM_Length
 SE_Startup_region_ROM (rx) : ORIGIN = __ICFEDIT_SE_Startup_region_ROM_start__, LENGTH = SE_Startup_region_ROM_Length
 SE_ROM_region (rx) : ORIGIN = __ICFEDIT_SE_Code_nokey_region_ROM_start__, LENGTH = SE_ROM_region_Length
 SE_IF_region_ROM (rx) : ORIGIN = __ICFEDIT_SE_IF_region_ROM_start__, LENGTH = SE_IF_region_ROM_Length
 SB_ROM_region (rx) : ORIGIN = __ICFEDIT_SB_region_ROM_start__, LENGTH = SB_ROM_region_Length
 SE_RAM_region (xrw) : ORIGIN = __ICFEDIT_SE_region_RAM_stack_top__, LENGTH = SE_RAM_region_Length
 SB_RAM_region (xrw) : ORIGIN = __ICFEDIT_SB_region_RAM_start__, LENGTH = SB_RAM_region_Length
}
 

  • Adjusted the UART in the sfu_low_level.h (this is the correct UART for the discovery and I already checked, that I get an ouput in an example project):
#define SFU_UART USART2
#define SFU_UART_CLK_ENABLE() __HAL_RCC_USART2_CLK_ENABLE()
#define SFU_UART_CLK_DISABLE() __HAL_RCC_USART2_CLK_DISABLE()
 
#define SFU_UART_TX_AF GPIO_AF7_USART2
#define SFU_UART_TX_GPIO_PORT GPIOA
#define SFU_UART_TX_PIN GPIO_PIN_2
#define SFU_UART_TX_GPIO_CLK_ENABLE() __HAL_RCC_GPIOA_CLK_ENABLE()
#define SFU_UART_TX_GPIO_CLK_DISABLE() __HAL_RCC_GPIOA_CLK_DISABLE()
 
#define SFU_UART_RX_AF GPIO_AF7_USART2
#define SFU_UART_RX_GPIO_PORT GPIOA
#define SFU_UART_RX_PIN GPIO_PIN_3
#define SFU_UART_RX_GPIO_CLK_ENABLE() __HAL_RCC_GPIOA_CLK_ENABLE()
#define SFU_UART_RX_GPIO_CLK_DISABLE() __HAL_RCC_GPIOA_CLK_DISABLE()
  • I changed the toolchain settings:

0693W00000HpvhlQAB.png0693W00000HpvieQAB.png 

  • In the app_sfu.h i activated the SECBOOT_DISABLE_SECURITY_IPS for debugging.

The thing is, I am not able to debug (I think this is normal, but I tought with the SECBOOT_DISABLE_SECURITY_IPS flag, I would be able to do that), since the fw directly goes into the hardfault at bootup. Also when I do the 2 power cycles as described in the AN5056, I never get a terminal output.

How can I check, that the SBSFU is correctly installed?

Edit:

Ok, I optimized for debug and can no see where it happens:

0693W00000HpvsAQAR.pngSeems to be a problem with the ROM region

This topic has been closed for replies.

1 reply

Bubbles
ST Employee
Jan 4, 2022 10:44 AM UTC

Hi @STsch.1​ ,

apparently SECoreBin initialization fails. When you changed the build settings for debug, maybe the code size increased and you need to revisit the linker settings.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.