Skip to main content
aheri.1
Visitor II
May 19, 2022 6:47 AM UTC
Question

Hi, After multiple tries of connecting STM32G031 MCU on target board with ST-link v2 using STMCubeProgrammer IDE, at one instant found an error window as pasted below. If in case TrustZone is enabled on this, is there a way out to erase the MCU?

0693W00000NqFIQQA3.png

This topic has been closed for replies.

1 reply

Bubbles
ST Employee
May 20, 2022 1:31 PM UTC

Hi @aheri.1​ ,

the G0 MCU doesn't support TrustZone, so the problem is probably something else. Try checking if the MCU power supply is correct and try connecting under reset.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.