Skip to main content
DFell.1
Associate II
March 18, 2022
Solved

Hello, I'm using an STM32H750 MCU where I'm integrating the Crypto lib v4.0.1 I would like to execute this library (.text) from a specifc section. But I can manage to do what I want.

You can found below a extract of my linker script:

MEMORY
{
 D1_CODE_RAM (xrx) : ORIGIN = 0x24070000, LENGTH = 64K
 FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128K
 NVRAM (rx) : ORIGIN = 0x8020000, LENGTH = 64K
}
 
.ram_code_load () :
{
 . = ALIGN(4);
 _sdata = .; /* create a global symbol at data start */
 *(.ram_code_load)
 *(.ram_code_load*)
 *RestApiServer.o (.text .text*)
 *Cryptographic_CM7.a:*(.text .text*)
 
 KEEP(*(.ram_code_load))
 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */
} >D1_CODE_RAM AT> NVRAM

What I expect is to found into my .map file the Cryptographic_CM7 .text code placed at 0x8020000 as it's done with RestApiServer.o code.

What I get is the Cryptographic_CM7 library .text code placed at 0x8000000...

Until now I had follow this PDF as ressources whitout any sucess. https://www.st.com/resource/en/application_note/an4296-use-stm32f3stm32g4-ccm-sram-with-iar-embedded-workbench-keil-mdkarm-stmicroelectronics-stm32cubeide-and-other-gnubased-toolchains-stmicroelectronics.pdf

Could someone provide me some help ?

This topic has been closed for replies.
DFell.1
DFell.1Best answer
Associate II
April 14, 2022

Finally I manage to understand what was happening,

The code as shared is working properly, but in the full file I do have between line 6 and 8 (in the example above) the following line:

 .text :
 {
 . = ALIGN(4);
 *(.text) /* .text sections (code) */
 *(.text*) /* .text* sections (code) */
 . = ALIGN(4);
 } >FLASH

Since this line has been defined before the definition of the .ram_load_code section all the .text has been located into the FLASH region and not the NVRAM as wanted.

1 reply

DFell.1
DFell.1AuthorBest answer
Associate II
April 14, 2022

Finally I manage to understand what was happening,

The code as shared is working properly, but in the full file I do have between line 6 and 8 (in the example above) the following line:

 .text :
 {
 . = ALIGN(4);
 *(.text) /* .text sections (code) */
 *(.text*) /* .text* sections (code) */
 . = ALIGN(4);
 } >FLASH

Since this line has been defined before the definition of the .ram_load_code section all the .text has been located into the FLASH region and not the NVRAM as wanted.