Skip to main content
Associate II
Jul 20, 2025 9:35 AM UTC
Question

HardFault error happens in case SFU_ISOLATE_SE_WITH_MPU is not used

In current, I am using the NUCLEO-H753ZI of STM32CubeExpansion_SBSFU_V2.7.0 demo project.

Hardfault error happens in SFU_SE_STACK_Clean api in case SFU_ISOLATE_SE_WITH_MPU is not used like "#undef SFU_ISOLATE_SE_WITH_MPU"

the value of sp is 0.

Please let me know how to resolve this issue.

static void SFU_SE_STACK_Clean(void)
{
  uint32_t sp_base = SE_REGION_RAM_START;
  uint32_t sp_top = SE_REGION_RAM_STACK_TOP;
  uint32_t sp = __get_MSP();
TRACE("\r\n= [SBOOT-MWU] SFU_SE_STACK_Clean[0x%08x]",sp);
 
  if ((sp > sp_base) && (sp <= sp_top))
  {
    while (sp_base < sp)
    {
      *(__IO uint32_t *)sp_base = 0U;
      sp_base += 4U;
    }
  }
  else
  {
    /*  error trigger a reset */
    HAL_NVIC_SystemReset();
  }
}
This topic has been closed for replies.