Skip to main content
YS.1
Visitor II
May 4, 2023 8:07 AM UTC
Question

Generating Option Byte .s19 file

Hi,

I need to generate option byte file(.s19) which is enabled Read out Protection for STM32F4.

The reason is to program this .s19 file using non ST programmer in production environment.

May i which ST Tool should i used to generate option byte file(.s19) ?

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
May 4, 2023 3:17 PM UTC

Welcome, @YS.1​, to the community!

There is probably no point in trying to put the Option Bytes in an S19, the reason for this has already been discussed here.

Instead, you should consult your programmer's documentation and find out how to use it to set the Option Bytes on the Command Line.

Hope that helps?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.