Skip to main content
tomptz
Associate
Feb 6, 2020 9:32 AM UTC
Question

For a new line of products, we are considering STM32F750 but it lacks on-the-fly decryption support. Is there a new line of microcontrollers planned that matches the spec of STM32F750 but includes support for on-the-fly decryption

We need a powerful M7 core running at high speed + GPU support for TouchGFX. It seems that STM32F750 is a perfect match, apart from the fact that it is missing support for on-the-fly decryption (OTFD). As we would like to use external flash memory and encrypt it, we will need OTFD support. I know that the new STM32 models that are launched have it on board. Is there a launch planned for a model similar to F750 but with OTFD support?

This topic has been closed for replies.