Skip to main content
Associate
Jan 31, 2025 3:24 PM UTC
Question

Failing to implement HAL_PKA_ECCCompleteAddition correctly

Hi,

I am struggling to get `HAL_PKA_ECCCompleteAddition` implemented correctly, that is, if I'm comparing the projective coordinates with a reference implementation, the results don't match. Same goes for converting the projective coordinates back to affine coordinates using `HAL_PKA_ECCProjective2Affine`. 

I am using a STM32u585vi microprocessor, and was able to use `HAL_PKA_ECCMul` properly already.

 

See below the function that shows incorrect results. Could you please provide help to proceed here?

ps. In its current form, the projective X coordinate produces equal results as a C# BountyCastle reference implementation. 

 

 

bool ecc_secp256r1_add_points_projective(const generator_point_t* p1, const generator_point_t* p2, generator_point_t* pOut) {
 const uint8_t Z_projective_input[prime256v1_Prime_len] = {[0] = 0, [31] = 1};

 uint8_t X[prime256v1_Prime_len];
 uint8_t Y[prime256v1_Prime_len];
 uint8_t Z[prime256v1_Prime_len];

 PKA_ECCCompleteAdditionInTypeDef eccAddInput = {
 .modulusSize = prime256v1_Prime_len,
 .modulus = prime256v1_Prime, // Curve prime
 .coefA = prime256v1_absA, /* PKA operation need abs(a) */
 .coefSign = prime256v1_A_sign, // Coefficient sign
 .basePointX1 = p1->x,
 .basePointY1 = p1->y,
 .basePointZ1 = Z_projective_input,
 .basePointX2 = p2->x,
 .basePointY2 = p2->y,
 .basePointZ2 = Z_projective_input,
 };

 if (HAL_PKA_ECCCompleteAddition(&hpka, &eccAddInput, HAL_MAX_DELAY) != HAL_OK) {
 return false;
 }

 PKA_ECCCompleteAdditionOutTypeDef eccAddOutput = {
 .ptX = X,
 .ptY = Y,
 .ptZ = Z,
 };
 HAL_PKA_ECCCompleteAddition_GetResult(&hpka, &eccAddOutput);

 // This is an effort to convert the coordinates manually, which failed, and I want to use the hardware acceleration
 // if (ecc_convert_to_affine(X, Y, Z, pOut->x, pOut->y) == false) {
 // return false;
 // }

 {
 PKA_MontgomeryParamInTypeDef montgomeryParamIn = {
 .size = prime256v1_Prime_len,
 .pOp1 = prime256v1_Prime,
 };

 if (HAL_PKA_MontgomeryParam(&hpka, &montgomeryParamIn, HAL_MAX_DELAY) != HAL_OK) {
 return false;
 }
 }

 uint32_t montgomeryparam[8] = {0};

 HAL_PKA_MontgomeryParam_GetResult(&hpka, montgomeryparam);

 /**
 After performing the ECC addition or other operations, we need to normalize the resulting point from
 projective coordinates to affine coordinates.
 */

 {
 PKA_ECCProjective2AffineInTypeDef eccNormalizeInput = {
 .modulusSize = prime256v1_Prime_len,
 .modulus = prime256v1_Prime, /*!< pointer to curve modulus value p */
 .basePointX = X, /*!< pointer to curve base point coordinate x */
 .basePointY = Y, /*!< pointer to curve base point coordinate y */
 .basePointZ = Z, /*!< pointer to curve base point coordinate z */
 .pMontgomeryParam = montgomeryparam, // secp256r1_R2_mod_p,
 };

 HAL_PKA_ECCProjective2Affine(&hpka, &eccNormalizeInput, HAL_MAX_DELAY);

 PKA_ECCProjective2AffineOutTypeDef eccNormalizeOutput = {
 .ptX = pOut->x,
 .ptY = pOut->y,
 };

 HAL_PKA_ECCProjective2Affine_GetResult(&hpka, &eccNormalizeOutput);
 return true;
 }
}

 

 

 

This topic has been closed for replies.

3 replies

ST Employee
Feb 3, 2025 11:02 AM UTC

Hello @MaartenMJR ,

After a quick look to the code you are providing and I'm wondering if X Y Z buffers to output results should be based as addresses as the .ptX and .ptY should get a pointer as parameter.

Can you check the implementation of STM32CubeU5/Projects/B-U585I-IOT02A/Examples/PKA/PKA_ECCProjective2Affine at main · STMicroelectronics/STM32CubeU5
as a reference for your implementation?
Also, could you provide the source of test vectors you are using to test this function?
Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Feb 5, 2025 8:30 AM UTC

Thanks for your response, and the (Montgomery) implementation reference (see below about that).

For a reference I use 2x multiplication of the generator base point, see below snippet. `double_origin_expected` gives the same results as in a python implementation. However, the `ecc_secp256r1_add_points_projective` does not give the same results.

// Multiply generator base point with 2, and compare with (base point + base point)

generator_point_t double_origin_expected;
const uint8_t scalar_2[prime256v1_Order_len] = {[31] = 2};

assert(ecc_secp256r1_multiply_base((buffer_view_t){.buffer = scalar_2, .size = sizeof(scalar_2)},
&double_origin_expected) == true);

const generator_point_t* const generator_origin = (generator_point_t*)&prime256v1_Generator[1];
generator_point_t double_origin;

//assert(ecc_secp256r1_add_points_affine(generator_origin, generator_origin, &double_origin) == true);
assert(ecc_secp256r1_add_points_projective(generator_origin, generator_origin, &double_origin) == true);

assert(memcmp(double_origin_expected.x, double_origin.x, sizeof(double_origin.x)) == 0);
assert(memcmp(double_origin_expected.y, double_origin.y, sizeof(double_origin.y)) == 0);


With the provided reference I'm able to verify that the computation of the MontgomeryParameter is correct:

{
const uint32_t input1_1PKA_ECC_ConvToAffine_IN_MONTGOMERY_PARAM[] = {0x00000001, 0x00000000, 0x00000002,
0x00000000, 0x00000002, 0x00000000};

const uint8_t prime192v1[] = {0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xfe, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff};

// Test montgomery param
{
PKA_MontgomeryParamInTypeDef montgomeryParamIn = {
.size = sizeof(prime192v1),
.pOp1 = prime192v1,
};

assert(HAL_PKA_MontgomeryParam(&hpka, &montgomeryParamIn, HAL_MAX_DELAY) == HAL_OK);
}

uint32_t montgomeryparam[sizeof(input1_1PKA_ECC_ConvToAffine_IN_MONTGOMERY_PARAM) / sizeof(uint32_t)] = {0};

HAL_PKA_MontgomeryParam_GetResult(&hpka, montgomeryparam);

assert(memcmp(montgomeryparam, input1_1PKA_ECC_ConvToAffine_IN_MONTGOMERY_PARAM, sizeof(montgomeryparam)) == 0);
}


Still I can't figure out why the `ecc_secp256r1_add_points_projective` computation remains faulty. Any ideas?

Associate
Feb 5, 2025 9:07 AM UTC

Note: In this example, the `Y` coordinate in ecc_secp256r1_add_points_projective is correct, but the `X` and `Z` coordinates not, and of course the affine result is then also incorrect.