Skip to main content
Associate
Jun 30, 2023 3:21 PM UTC
Question

Executing an application directly from RAM rather than the flash memory - SBSFU.

We currently utilize the STM32H7B0xB microcontroller, which offers 1.4 MBytes of RAM and 128KBytes of flash memory. While exploring the SBSFU examples found examples for running from external flash directly, I could not locate one that specifically demonstrates running the application from the RAM region for SBSFU. Is it supported?

This topic has been closed for replies.

2 replies

MM..1
Super User
Jun 30, 2023 5:13 PM UTC
HotaruAuthor
Associate
Jul 1, 2023 8:46 PM UTC

Thanks @MM..1  for running the code from RAM. However, I was looking at secure boot and if SBSFU supports apps running app after doing a signature verification and decryption.