Skip to main content
Associate II
December 19, 2023
Solved

Error occured while provisioning '.obj files' on STM32H573-DK

hello 

 

I'm using a STM32H573-DK board for engineering samples. 
so. I'm run a example this link but provisioning.bat files does not run at 'Step 3 : Provisioning'

How to fix this problem?

 

provnn_step3.PNG

 

 

This topic has been closed for replies.
Frantz LEFRERE
Frantz LEFREREBest answer
ST Technical Moderator
December 19, 2023

This is a material switch on your board, bottom left not far from RESET. Thre is a serigraphy : BOOT0

6 replies

ChoppaAuthor
Associate II
December 19, 2023

attach obkey_programming.log file contents


C:\Users\user\STM32Cube\Repository\STM32Cube_FW_H5_V1.1.1\Projects\STM32H573I-DK\ROT_Provisioning\OEMiROT>call ../env.bat
Configure OBKeys HDPL1-DA config area
-------------------------------------------------------------------
STM32CubeProgrammer v2.15.0
-------------------------------------------------------------------

ST-LINK SN : 000600164D46501220383832
ST-LINK FW : V3J13M4
Board : STM32H573I-DK
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x484
Revision ID : Rev A
Device name : STM32H5xx
Flash size : 2 MBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0xFF
SFSP Version: v0.0.0
Debug in Low Power mode enabled


Hard reset is performed
-------------------------------------------------------------------
STM32CubeProgrammer v2.15.0
-------------------------------------------------------------------

ST-LINK SN : 000600164D46501220383832
ST-LINK FW : V3J13M4
Board : STM32H573I-DK
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x484
Revision ID : Rev A
Device name : STM32H5xx
Flash size : 2 MBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0xFF
SFSP Version: v0.0.0
Debug in Low Power mode enabled

ST-LINK SN : 000600164D46501220383832
ST-LINK FW : V3J13M4
Board : STM32H573I-DK
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x484
Revision ID : Rev A
Secure Data Provisioning Start. OBK Input file : ../DA/Binary/DA_Config.obk
Error: Execution of RSS CMD fail with timeout
Error: call_RSSLIB_SetOBKey Failed
лллллллллллллллллллллллллллллллллллллллллллллллллл 100%Error:
OBKey Provisioning failed

 

Frantz LEFRERE
ST Technical Moderator
December 19, 2023

Hello,

insure to change SW has indicate in the trace and then it should works

Br,

Frantz 

ChoppaAuthor
Associate II
December 19, 2023

Hello LEFRERE.


how to change SW?
Can i see trace and working SW, if i change SW?

 

 

 

 

Frantz LEFRERE
Frantz LEFREREBest answer
ST Technical Moderator
December 19, 2023

This is a material switch on your board, bottom left not far from RESET. Thre is a serigraphy : BOOT0