Skip to main content
STLearner
Associate III
Nov 16, 2022 6:35 AM UTC
Question

Enquiry on STM32G4

Looking for the MCU specs with the following key requirements:

              - 24 IO : 8 input, 8 outpt, 8 x LEDs

              - secure boot features

              - hardware reset

- backline support – CAN Bus communication at 5V

Can STM32G4 support above mentioned features?

This topic has been closed for replies.

1 reply

Bubbles
ST Employee
Nov 16, 2022 10:27 AM UTC

When looking for an ideal MCU for your application try using the CubeMX application. You can filter the whole STM32 by parameters.

In this case it mostly depends how secure should the booting be. STM32G4 has some basic security, but for true secure boot you may need STM32L5. See AN5156 for more information about STM32 security.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.