Skip to main content
Associate III
Jun 17, 2024 5:20 AM UTC
Question

Encryption using AES CCM + MIC - stm32wb

Hi,

i am trying to develop a device which sends out bthome advertisements via ble (some sensor data).

So far so good, this part is working, but now i would also like to use bthome encryption.

https://bthome.io/encryption/

So following this guide, i would need AES128 - CCM and MIC.

What i did so far is enabling AES and set it to be CCM and added a key (using CubeMX).

In the generated code i now have the hcrypt handle.

What i did afterwards -> I collected all the described data to create the nonce:

 uint8_t nonce[13];
 // MAC Address
 nonce[0] = mac_address[0];
 nonce[1] = mac_address[1];
 nonce[2] = mac_address[2];
 nonce[3] = mac_address[3];
 nonce[4] = mac_address[4];
 nonce[5] = mac_address[5];

 // add bt_home_device_info
 nonce[6] = bt_home_device_info;

 // add UUID
 nonce[7] = (uuid >> 8) & 0xff; 
 nonce[8] = uuid & 0xff; 

 // add counter
 nonce[9] = (counter >> 24) & 0xff;
 nonce[10] = (counter >> 16) & 0xff;
 nonce[11] = (counter >> 8) & 0xff;
 nonce[12] = counter & 0xff;

This is my nonce i would need for AES CCM.

Now sadly the example on bthome is a python one.. but they are using it as follows:

from Cryptodome.Cipher import AES

cipher = AES.new(key, AES.MODE_CCM, nonce=nonce, mac_len=4)
ciphertext, mic = cipher.encrypt_and_digest(data)

So basically a new cipher instance is created with the key and the nonce, telling the mac/mic len is 4 bytes.

Then encrypt the data (bthome service data) with this cipher.

My question is how i would achieve this using HAL_Cryp* library on a stm32wb55?

I looked for different examples and there are some for a wb55 but none for CCM as far as i can see.

-> Then i saw that there also is a third party software pack mbedtls which should make this a bit easier but apparently it is not available on stm32wb.

My current aes init is as cubemx generated it:

CRYP_HandleTypeDef hcryp1;
__ALIGN_BEGIN static const uint32_t pKeyAES1[4] __ALIGN_END = {
 0xAAAAAAAA,0xBBBBBBBB,0xCCCCCCCC,0xDDDDDDDD};
__ALIGN_BEGIN static const uint32_t HeaderAES1[4] __ALIGN_END = {
 0x00000000,0x00000000,0x00000000,0x00000000};
__ALIGN_BEGIN static const uint32_t B0AES1[4] __ALIGN_END = {
 0x00000000,0x00000000,0x00000000,0x00000000};

/* AES1 init function */
void MX_AES1_Init(void)
{

 /* USER CODE BEGIN AES1_Init 0 */

 /* USER CODE END AES1_Init 0 */

 /* USER CODE BEGIN AES1_Init 1 */

 /* USER CODE END AES1_Init 1 */
 hcryp1.Instance = AES1;
 hcryp1.Init.DataType = CRYP_DATATYPE_8B;
 hcryp1.Init.KeySize = CRYP_KEYSIZE_128B;
 hcryp1.Init.pKey = (uint32_t *)pKeyAES1;
 hcryp1.Init.Algorithm = CRYP_AES_CCM;
 hcryp1.Init.Header = (uint32_t *)HeaderAES1;
 hcryp1.Init.HeaderSize = 4;
 hcryp1.Init.B0 = (uint32_t *)B0AES1;
 hcryp1.Init.DataWidthUnit = CRYP_DATAWIDTHUNIT_WORD;
 hcryp1.Init.KeyIVConfigSkip = CRYP_KEYIVCONFIG_ALWAYS;
 if (HAL_CRYP_Init(&hcryp1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN AES1_Init 2 */

 /* USER CODE END AES1_Init 2 */

}

My knowledge about crypto is quite limited so i also don't really know what i should use for B0 and HeaderAES1.

Maybe you know some wrapper library or sth. similar which i could use.

This topic has been closed for replies.